Part Number: TMS320F280049C-Q1
Tool/software:
Hi Champs,
Could you help to check the maximum input current of below pin? Is there a risk if the input current reaches 45A?

Thanks!
Best regards,
Julia
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049C-Q1
Tool/software:
Hi Champs,
Could you help to check the maximum input current of below pin? Is there a risk if the input current reaches 45A?

Thanks!
Best regards,
Julia
Hi Julia,
Is there a risk if the input current reaches 45A?
Is this a typo?
Pasting datasheet specifications below.

Best Regards,
Ben Collier
Hi Ben,
Yes, this is a misunderstanding described by customer. The 45A is converted into a voltage signal and input to the ADC pin after processing.
So the maximum input current is 20mA. If the input exceeds 20mA, what will happen to the F280049? Will it reset or will it damage the chip?
Thanks!
Best regards,
Julia
Julia,
If the input exceeds 20mA, what will happen to the F280049? Will it reset or will it damage the chip?
The chip will be damaged.
Also please see in the notes that the maximum continuous current is 2mA.
Best Regards,
Ben Collier