Other Parts Discussed in Thread: CONTROLSUITE, MOTORWARE
Tool/software:
Greetings,
We have purchased the TMDSHVMTRINSPIN development board and the 200V PMSM that's supposedly compatible with it. However, for a 230V AC input from the wall mains, the rectified output is around 313 V DC and even if we bypass the PFC, the 313 DC Bus voltage will not be appropriate for the 200 V PMSM. What options do we have to run this motor now?
If we use a lower rated external DC-supply, then would that imply also reprogramming (designing) the PFC switching signals?
Thanks
Best Regards