Tool/software:
TI:
I am trying to make a small connector to our target board from the connections on the stand-alone XDS110 probe using the CTI-20 connector . On figure 6-30 of the TMS320F28P65x datasheet, it shows the connections to the processor from the 20 pin JTAG header. However, in the LaunchPad demo board, the on-board XDS110 has two additional lines that run to two Serial Communications Lines (TX/RX). Are these connections important and, if so, how should they be connected to the stand-alone XDS110 Probe?
Thank you,
David