This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650SK: about the external adc voltage ref design

Part Number: TMS320F28P650SK
Other Parts Discussed in Thread: REF3430

Tool/software:

Dear Forum Members,

I am designing a system using the TMS320F28P650SK MCU with its internal 16-bit ADC. Currently, I plan to use the REF3430 (3.0V output) as the voltage reference. Could you please advise on the following:

1.Should I add a buffer to improve drive capability, especially if the ADC samples at high speed.

2 How to choose an OA.

3.Below is a circuit diagram, is it available or any suggestions.

Thanks!

song