Part Number: LAUNCHXL-F28069M
I am studying the theory of brushless electric motors and do not understand how to calculate the torque delivered by a motor. Let's assume a PMSM brushless motor using a FOC.
I found these three formulas:
---------------------------------------------------------------------------------------------------------------
- T = I[Arms] * Kt[Nm/Arms]
1) here is the I[Arms] the one I measure with a current probe on one of the three phases of the motor? Or is the current Iq quadrature? Kt is on the motor's datasheet
---------------------------------------------------------------------------------------------------------------
- Torque (Newton-Meters) = Rotor Flux (Webers) * Iq (Amps) * Rotor Magnet Poles * (3/4)
2) what changes between this formula and the previous one? Do both lead me to the same result?
---------------------------------------------------------------------------------------------------------------
- T = 8,3 * Iphase / Kv
3) This is another formula found online that use Kv, not Kt!.. again, what changes between this formula and the previous ones? Do I get the same result?
---------------------------------------------------------------------------------------------------------------
4) In the formulas I have used I always have doubts about what current I should enter (whether phase or quadrature current). If I were to use Iq but I don't know it and have no way to calculate it, then I would have no other way to find the torque?