Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE,
Hello,
I want to develop an own bootloader for CPU1.
I can use the software reset without a connected Debugger. This works.
With Debugger I want to use the emulation register. But it seems that this doesn't work.
I use CCS v20, C2000Ware v6, TMS320F28388D control card, on board Debugger.
S2 is switched to Flash boot. S1 without debugger -> software Reset works
I want to debug my programm with S1 enabled Debugger.
I want to emulate the Flash Boot with start on section 0.
It seems at the moment, that the ROM bootloader runs in Wait Boot.
Additional question, but not relevant at the moment:
Do I use the same register with adapted values to create a Reset with start from RAM on the CPU2?
Thank you
Best regards
Steffen Rose
Thank you