This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FFT code example

Hi

I am going to implement 128 point FFt on control stick kit TI28069 using code composer studio v4 . For the sake of simplicity I copied a part of  the code example  SineFIRFFT32-Main.c  from controlsuit package. As far as I know the only header file I need to add other than default headers is FPU.h which I added so for headers files section, I have :

#include"PeripheralHeaderIncludes.h"

#include"F2806x_EPwm_defines.h"     // useful defines for initialization

#include"F2806x_DefaultISR.h"

#include"FPU.h"

#include <math.h>

However, when I run my codes I get the following error

undefined             first referenced      

symbol in file

---------             ----------------      

_RFFT_f32             ./TriggeredADC-Main.obj

_RFFT_f32_mag         ./TriggeredADC-Main.obj

_RFFT_f32_sincostable ./TriggeredADC-Main.obj

error: unresolved symbols remain

error: errors encountered during linking; "TriggeredADC.out" not built

 

 

 Based on my past experience it means some library related to FFT has not been added or defined correctly. So is there any other library I have to add? Can you help me regarding this issue?

Thanks

 seyed