hi,
i had create a project with the "Header Files and Peripheral Examples"
and the project works fine, but when i call _iqsine(xxx) the project dosn´t run and the linker gives me the following errors:
warning: entry-point symbol "_c_int00" undefined
undefined first referenced
symbol in file
--------- ----------------
FS$$ADD C:\\xxx\\Debug\\pid_reg3.obj
FS$$CMP C:\\xxx\\Debug\\pid_reg3.obj
FS$$DIV C:\\xxx\\Debug\\Test_CCS3_3_PFC.obj
FS$$MPY C:\\xxx\\Debug\\DSP2803x_CpuTimers.obj
FS$$SUB C:\\xxx\\Debug\\pid_reg3.obj
FS$$TOL C:\\xxx\\Debug\\DSP2803x_CpuTimers.obj
FS$$TOU C:\\xxx\\Debug\\Test_CCS3_3_PFC.obj
U$$TOFS C:\\xxx\\Debug\\Test_CCS3_3_PFC.obj
error: unresolved symbols remain
error: errors encountered during linking; "./Debug/Test_CCS3_3_PFC.out" not
built
It is the same code, the only change is the iqmath call but i don´t know whats wrong...
What can i do, where are the mistake ?
I don´t like to use the cla, the project have to run on a smaller chip later.
MfG Chris