Other Parts Discussed in Thread: TMS320F28335
Hi,
We are working on a 28335 with the ezdsp kit, with the ultimate goal of running a 4096pt FFT to essentially work as a frequency counter. We wish to determine the frequency of a few pulsing signals that are in the range of 150MHz-152MHz. We have mixed the signal to 0-2MHz (baseband). We need to sample at 4MHz minimum (Nyquist). To get started we are using some of the example ADC codes from the library we do get some results but upon attempting to plat these resutls we get values such as 4.3 x 10^43 on both axes, which are just ridiculous numbers. We arent sure if there is a problem with our setup our simply with our graph display parameters. We also have the FFT library but would love some more info/code to help move us along, we are just students however with little to no background in any of this and are struggling to say the least. Any potential aid would be greatly appreciated if anyone has any thoughts/ideas/code/samples that could be beneficial.
Please and Thanks you,
Chris & Trent