I have two files that I am unable to find: "FlashAPIInterface28335V2_10.out" and "rts2800_fpu32.lib"
//----
I believe that the newest version of the FlashAPI for the 28xx parts is v2.10. Using "Tools->F28xx On-Chip Flash Programmer", I receive the Flash Programmer Settings Dialog. The bottom of this dialog box has a prompt "Select version of Flash API Interface file:". The default selection is "FlashAPIInterface28335V2_10.out", though the file does not exist on my system. I have uninstalled and reinstalled the entire CCS toolchain. The only version of the file I do have is "FlashAPIInterface28335V1_01.out". Clearly, this is not the latest version. I am unable to find any other versions.
The second file, a runtime support library, has been referred to in TI documentation, though I am unable to locate a copy of it. I do have rts2800_ml.lib as well as "rts2800_fpu32_fast_supplement.lib".
//----
When connecting to the target that I have just flashed using "FlashAPIInterface28335V1_01.out", I often get the error message:
Trouble Setting Breakpoint with the Action "Terminate Program Execution" at 0x33858d: Error 0x00000008/-1076 Error during: Break Point, Cannot set/verify breakpoint at 0x0033858D
Breakpoint Manager: Retrying with a Legacy Hardware breakpoint
If I get a clean connect, I certainly get the above error message when loading the same .out file that I flashed the part with.
Placing a breakpoint in main() after receiving this error simply produces another and performing a run...halt yields a PC out in the middle of nowhere.
The application I am trying to use is the flash example from TI, unmodified. All RAM-based examples work just fine.
//----
I have downloaded and installed the following:
"Code_Composer_Studio_v3.3_Build_3.3.38.2_FET"
"ActivePerl-5.8.9.825-MSWin32-x86-288577.msi" <-- ActivePerl 5.8.9, which is a pre-requisite forBIOS
"bios_setupwin32_5_33_03.exe" <-- BIOS
"F2823x_RevA_CSP.exe" <-- chip support package for revA silicon, which I do not have
"F2823x_CSP_v3.3.2501.exe" <-- chip support package for 2823x and 2833x devices
"SR12_CCS_v3.3_SR_3.3.82.10.1.exe" <-- service release 12
"C2000CodeGenerationTools5.1.3.exe" <-- latest version of code generation tools
"sprc539.zip" <-- Flash2833x API V210
"BHEMU-SetupCCS_v3.3.300.0.zip" <-- latest BlackHawk emulator drivers for the BH-USB-2000 device I am using
//----
Windows XP, SP2 -- 2GB ram
//----
Hardware is a 28335 ControlCard mounted on a custom PCB with 1.25" traces for the JTAG. No vias are present between any JTAG connections and the DIMM connector. Supply rails are quiet.
//----
The toolchain versions identified in the "Help->About" and subsidiary "Component Manager":
CCS-FET 3.3.82.10
IDE 5.98.0.393
BIOS 5.33.03
Code Generation Tools 5.1.3
F28xx On-Chip Flash Programmer 5.92.0.316