Hi,
I have created my own board with a Concerto processor. The reset circuit I'm using is the same as the DIMM 100 example. I have 2.21K pull-up resistors and 0.1uF caps tied to the /XRS and /ARS pins.
I have tested 10 boards. Four of them work correctly and I measured 3.3V on the reset pins.
Six of the boards will not allow me to program them with my XDS510 emulator.
They will sometimes fail with an error message about being held in reset, and other times they will go through the steps in the GEL file until M3_Ram_Init is called and then they get forever stuck in a while loop. On these six boards I'm measuring 2.8V on the reset pins.
I can only assume that these pins are acting as outputs for some reason, otherwise they should be getting pulled up to 3.3V. Right?
What can cause this? I can't find documentation about when and why these pins are outputs.
Thanks,
Joel