This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding Code generation error

Hello,

I am using F2808, FOC control of an Induction motor. I am using simulink(embedded coder)to develop the code for the DSP. I created the linking between simulink and code composer studio using Xmakefilesetup. later I installed F280x Digital Motor Control Library. Is the DMC and IQ math library are automatically used while code generation????

Are do i need to link them????because I am getting warnings like..

http://img827.imageshack.us/img827/3480/rpj3.jpg

thanks in advance.

Is it the Block Park transformation is creating the error..???