This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Learning remaining and used memory space for TMS320F28335 using CCS v5

Other Parts Discussed in Thread: TMS320F28335

Hi,

I use TMS320F28335 microcontroller with CCS v5.4. 

After a code is compiled, I want to know the used and the remaining memory space.

For example, RAM : 40% used and 60% free

                         FLASH : 15% used and 85% free

Also, I analyzed the F28335.map file and it is attached.

I saw at this file that some memory space is used and some memory space is empty.

But I did not understand it very well.

Please help me at this subject.

7652.F28335.rar