Hello,
I acquired the experimental kit TMDSDOCK28335 and started programming based on "Flashing Leds" program included in the Control Suite. My target with this evaluation board is to generate a 12.5Mbps 14 bit-sequence and in paralell, sample it at 50MHz so as to detect the sequence.
As an attempt to start developing this idea, I tried to generate a square signal with a determinate bit rate using "Flashing Leds" code. To do so, I decreased CPUTimer0 and variable “Gui_LedPrd_ms” and the resulting square signal was the expected at low frequencies but as long as I decreased the CPUTimer0, I noticed that I was not able to generate periods lower than 1usec. I tried to disable B and C tasks of the background loop but it didn't work either. The rest of parameters (such as clock configurated at 150MHz) were the same as in the original "Flashing leds" project.
Can anyone give me some advise?
Thank you so much