Hi all,
There is a problem of Dual chip select problem.
I've used the EPI with the following settings now.
ECADR = 0x00
EPADR = 0x02
ERADR = 0x02
It is as follows when you check the TRM.
CS0 -> 0xC0000000, CS1 -> 0x80000000
However, the actual device(TMDSDOCKH52C1) is as follows.
CS0 worked when it is accessed to 0x80000000,
CS1 worked when it is accessed to 0xC0000000,
Description of the manual is correct?
Best regards,
FSSer