Other Parts Discussed in Thread: CONTROLSUITE
Hi,
I want to test a new PLL algorithm and current controller with TMDSSOLAR(P/C)EXPKIT. However, instead of (P/C) I need F28335. A problem is, I need scaling and offset parameters for analog inputs (AC voltage, AC current, DC voltage). It seems that for AC signal the offset is 1.65V (0x07FF). My best guess is, based on (P/C) code that max DC voltage is 39.97V and similar for AC voltage (40V). Unfortunately it is not clear if max value for AC current is 5A or less. It might be interesting to mention that I use external DC power supply (30V) and 240/15V transformer for grid connection. All protection is done (blocking diodes on DC side and fuse on AC side) .
Any help in this matter is much appreciated. Thank you in advance.
Regards,
Petar