Hello,
I'm working with BoosterPack + Launchpad in order to have a BLDC controller.
In the project, we need to support current of 35A to have maximum torque.
I am looking for alternatives to the current CSD18533Q5A transistor. I found the CSD18509Q5B component, in order to preserve the form factor. Is it the appropriate device? If the form factor is not a requirement, which would be an appropriate component to support bigger current?
I would also like to ask how to address the impact of resistors R28, R29, R30, R31, R32, R33 and capacitors C31, C32, C33.
Best regards,
Flavio