Hello, I need help choosing the best evaluation kit for our electric propulsion aircraft prototype. It is not clear from reading the pages of the instaSPIN technologies if insta FOC can give any advantages compared to insta-BLDC for given specifications.
Currently we are considering to test 3 motors for the prototype. Range of parameters about similar for all of them:
- All motors are brushless sensorless BLDC type, 2 are out-runners, 1 in-runner,
- number of poles : from 18 to 24
- kV from 40 rpm/v (direct drive) to 115 rpm/v (with reduction gear)
- max 20KW each
- rotational speed up to 9,000RPM , this is mechanical rotational speed, electronic (waveform) speed 81,000 to 108,000 respectively according to poles
- From 0 to 500RPM no load, from 500RPM to 9000RPM load gradually increases proportionally to the RPM of the propeller (rotational speed)
- max estimated torque on the shaft about 40Nm
- Working voltage 60v (for now although in the long run we want to use 85v battery).
- Maximum burst amperage for this range of power would be up to 250A or 300Amps (based on experience with other controllers)
- Continuous working amperage 150Amps
- In terms of the efficient usage of in-flight battery we need the most efficient waveforms (in efficient advance with rotor's position) to get most mechanical power from least battery current
- Proper directional motor' startup is important to match the propeller.
------------------
We are considering to start with either DRV8301-HC-C2-KIT to try instaSPIN-BLDC method or DRV8301-69M-KIT to try instaSPIN-FOC solution on all motors and in the end we will add power module to replace kit's simple MOSFET's pairs as well as add SPI communication with our in-flight monitoring micro-controller.
Which method/evaluation kit to choose? Is there more appropriate kit for this? Are they all equally good for this application? We'd prefer not to do any re-programming of the motor control but to use this part of TI solution as is. We'd only add communication with our in-flight controller. If both methods are the same we'd go with InstaBLDC method as it is easy to use .
Thanks in advance for any advice
Vlad