I am having troble interfacing the DAC8760 EVM module to DSP TMS320F28335 module through SPI communication because of the 24bit wide character of the DAC registers. DSP28335 only have 26bit character SPI communication. Later i wanted to make the DSP 28335 operate as master and two slave modules, ADS8332 and DAC8760. ADS8332 DSP28335 Communication already function correctly because of SPI 16bit communication but i wanted to add the DAC module to the embedded system but no luck because of the 24bit character SPI. Any suggestions for the interfacing of the DAC8760 to DSP28335? Thanks