Dear Support,
a few weeks ago, we buyed the LAUNCHXL-F28377S + BOOSTXL-DRV8301 Bundle and I am at the moment trying
to get it to work. At the Moment, we want to use the Boards for testing of an BLDC motor.
I would for that reason like to keep the whole thing as simple as possible, ideally with a GUI.
I know that there is the INSTASPIN Universal GUI and after a few tries I got it to work in CCS 6.1.
However, if I try to connect to the Launchpad via "connect Target" like it is said in the UNIVERSAL GUI QSG pdf-file from Motorware, I get the following error:
C28xx: Error connecting to the target: (Error -1041 @ 0x6) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 5.1.641.0)
I would like to know if this is actually the right GUI to use and/or if there is more detailed documentation and examples regarding this particular combination.
Thanks,
Johannes Monz