Hello,
I have two RDV8301EVM (w/ F28069 ISO Control Card) boards in my lab. I use one EVM board to drive a 3 phase sensorless motor. The PVDD connect to 24V which from 600W Power Supply. I run InstaSPIN_FOC_F2806x.exe app to drive this motor. When the Load of motor increase, the current also increase and PVDD keep to 24V (Both Current and Voltage value read from Power Supply Display). The current from Power Supply can reach to 10A when motor has max load and Voltage keep to 24V. The motor running fine at max load without any problem.
I change another EVM board, use same motor, setting and same Power Supply. When add load to motor, once the current reach to 1A then the Voltage ramp up to 26V ~ 34V rippled. The motor is still running but I didn't add load to increase current. Because I think some thing wrong in this EVM board. This EVM board work fine before but today I encounter this symptom. Now this EVM board can complete Identify Motor and running without load at low speed. But when I add load to 1A, the Voltage ramp up from 24V to above 30V. The Power Supply didn't damaged after I check it.
So, I need help to know where can I check or which parts in EVM board may damaged. Thanks in advance.