This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fatal error: could not open source file "MEMORY"

**** Build of configuration Debug for project openloop ****

 

F:\Texas Instruments\ccsv4\utils\gmake\gmake -k all

'Building file: ../DSP281x_GlobalVariableDefs.c'

'Invoking: Compiler'

"F:/Texas Instruments/ccsv4/tools/compiler/c2000/bin/cl2000" --cmd_file="F:\Texas Instruments\ccsv4\tools\compiler\c2000\lib\F2812_EzDSP_RAM_lnk.cmd"  -v28 -mt -ml -g --include_path="F:/Texas Instruments/ccsv4/tools/compiler/c2000/include" --include_path="F:/Texas Instruments/ccsv4/tools/compiler/c2000/include" --include_path="C:/Documents and Settings/Administrator.NITC-2ACBE34D84.002/My Documents/workspace/DSP281x_common/include" --diag_warning=225 --preproc_with_compile --preproc_dependency="DSP281x_GlobalVariableDefs.pp"  "../DSP281x_GlobalVariableDefs.c"

[MEMORY.]

>> WARNING: more than one source file is specified; preprocessor output will be generated for last file only

Fatal error: could not open source file "MEMORY"

1 fatal error detected in the compilation of "MEMORY".

Compilation terminated.

 

>> Compilation failure

gmake: *** [DSP281x_GlobalVariableDefs.obj] Error 1

'Building file: ../main.c'

'Invoking: Compiler'

"F:/Texas Instruments/ccsv4/tools/compiler/c2000/bin/cl2000" --cmd_file="F:\Texas Instruments\ccsv4\tools\compiler\c2000\lib\F2812_EzDSP_RAM_lnk.cmd"  -v28 -mt -ml -g --include_path="F:/Texas Instruments/ccsv4/tools/compiler/c2000/include" --include_path="F:/Texas Instruments/ccsv4/tools/compiler/c2000/include" --include_path="C:/Documents and Settings/Administrator.NITC-2ACBE34D84.002/My Documents/workspace/DSP281x_common/include" --diag_warning=225 --preproc_with_compile --preproc_dependency="main.pp"  "../main.c"

[MEMORY.]

>> WARNING: more than one source file is specified; preprocessor output will be generated for last file only

Fatal error: could not open source file "MEMORY"

1 fatal error detected in the compilation of "MEMORY".

Compilation terminated.

 

>> Compilation failure

gmake: *** [main.obj] Error 1

gmake: Target `all' not remade because of errors.

Build complete for project openloop

This is the console view when I try to compile my project in CCS v4. I was able to build and get an output file for the same in CCS v6. But I have an old eZDSP with only parallel port connection. I was not able to get the configuration for that in CCS v6. I have added every file I did in CCS v6 in the CCS v4. But it shows the above error. I have checked the search include paths and none of it contains double ". Please help me.

Murali Manohar