Other Parts Discussed in Thread: CONTROLSUITE
Hi, I am using the HVMotorCtrl+PfcKit to test a sensorless PMSM, I used the program HVPM_Sensorless in the folder ~controlSUITE\developent_kits\HVMotorCtrl+PfcKit_v2.0. I followed the instruction of the file "Sensorless FOC of PMSM.pdf". In BUILD LEVEL 6, I can drive the motor run in closed loop at low speed, but once I set the reference speed higher, the controller will enter error state and the motor stops, the LED1 and LED2 flush continuously.
An variac input power is used and the voltage I used is about 110 V, the controlCARD is TMS280F28035. I changed the RS, LS and poles value according the motor I tested, and the BUILDLEVEL is set to LEVEL6, nothing else changed in the program.
So why the system can work well in low speed but encounters error once the speed is set higher?