Hello,
We are using SpinTAC sensored to run a very high torque motor (450Nm). The variable gMotorVars.Torque_Nm is an _iq24 variable which means that the maximum value it can hold is +-128, right? and therefore it will overflow. If that is the case, what changes should I make to get a good Torque estimation?
Regards
Javier