Hello, both kits are based on C2000 MCU but InstaSPIN is offered up to F28069 while DesignDrive offered only with the latest and greatest F28377 MCU.
IT is not including InstaSPIN with DesignDrive/IDDK and I am getting confused with this spread of multiple solutions. Some version of FOC library is provided for IDDK/DesignDrive to drive motors but not InstaSPIN... I like that IDDK / TIDM-SERVODRIVE includes 3 types of the phase current sensing allowing to compare the results.
Why InstaSPIN is not included in the latest IDDK/DesignDrive software ?
What are the differences for the developer? My project is to drive motor (not a servo) 84v voltage 3 phase high power output BLDC 20kW experimenting with different number of coils/poles and with RPMs/volt... There is no executable program for IDDK similar to InstaSPIN helping to figure out the optimal motor parameters but there is library in DesignDrive and probably examples to play with motor... Will TI release another executable software for DesignDrive/IDDK similar to InstaSPIN?
Please share your thoughts about when and how to prefer one over the other to drive high power 3 phase BLDC motors with and without sensors.
Thanks in advance
Vladimir