hi: chris
how are you
I find ti has a new application . TIDA-00366.
can you find it's program of 28027 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi: chris
how are you
I find ti has a new application . TIDA-00366.
can you find it's program of 28027 ?
chris:
you know , in controlsuite , just HV has ACI motor control used F28035 program .
and has not program in Launchpad f28027 about ACI .
TIDA-00366 use F28027 control ACI motor . it is different . because of FLASH and RAM place with F28035.
Otherwise , F28027 has not QEP . how use it control speed when V/F modul ? dose it can FOC without QEP measure motor speed?
so , it is hard for F28027 control ACI motor . I want to know TIDA-00366 detail of program.
best regard
yanzheng FU
Question about this design, is it possible to use the AMC1301 + op amp current sense design and isolated drivers in tida-00366 for instaspin FOC? In the documentation it mentions delays induced by the design. Will it work or does the latency cause FAST to not function correctly? I have been trying to find a high accuracy in phase current sensing option but because I need up to around 120V I'm struggling to find a good solution.
we've never tried it, but it should work. the important part is triggering the sample at a specific time. you can have some delay in the conversion and communication.
have you looked into in phase current LEM sensors?
We have released an eval kit, IDDK (Industrial Drive Development Kit), which basically covers various options of grounding/ isolation, various current sensing options such as non-isolated shunt connected to inverter bottom half, or LEM and Sigma/Delta connected in series to motor phases. It is a good platform to study and compare the influence of various methods. Usually it is packaged with F28379D which has sigma delta modulator and differential ADC config (16b) as well. I would recommend you to review the link below for more information.
best regards,
ramesh
The delfino MCUs look fantastic for motor control, but wouldn't using one mean going without many of the features found in instaspin? Is the design drive sensorless software as capable as instaspin FAST? Would it be feasible to reuse F28069 motor profiling code using the control drive estimator instead of FAST or does the delfino software already have it's own motor profiling code?