Part Number: DRV8301-69M-KIT
Other Parts Discussed in Thread: MOTORWARE, DRV8301, DRV8305
Tool/software: Code Composer Studio
To whom it may concern,
I used the Motorware_Hal Tutorial to read the DRV8301-69M potentiometer and then wrote some of my own code to link the potentiometer reading to the IqRef_A variable.
When I turn my system on, it is fine unloaded. However when I turn the potentiometer to 100% and put some load on the system it just stops instead of resisting. I would have expected the current to increase all the way up to 36A to resist the load. For a video of what I mean, please seen video below:
Any help would be appreciated. I'm sure it's an issue with my PU scaling or something similar.
James