Other Parts Discussed in Thread: CONTROLSUITE
I'm unable to make sense of this.
Page 64 of the DS says load capacitance (CL1, CL2) must be 12 to 24pF.
Reading this literally, the recommended crystal load capacitance would be somewhere between 6 to 12pF, ignoring parasitics.
The crystal Q1 used in the LaunchPad (LAUNCHXL-F28377S) is as follows:
Mfg PN: ATS100B-E
Description: 10Mhz, +/-30ppm, 18pF, 60 Ohm, -40 to 85C
And of course, the dual load capacitors (C3, C4) used here are both 36pF correctly matching the 18pF load Capacitance of the crystal.
Is this crystal a bad choice or am I missing something? Are there any other recommended crystals?
Thanks - Adam