This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069: [eCAN] the activity of the local acceptance mask when LAMI bit field was clear.

Part Number: TMS320F28069

Hi Champs ,

Does the local acceptance filter will be work whatever the LAMI bit filed was 1 or 0 ?

At GAM register description , it shows the filter will not work when GAMI was 0/

According our experiment , the LAM will work  whatever LAMI was 1 or 0. 

However , customer would like to have double confirm since we did address it at datasheet,

Thanks

BR

Brian 

  • In the "0" description for the AMI bit (bit 31) of the CANGAM register, the following last 2 lines are incorrect:

    Filtering is not applicable. The MSGIDs must match bit-for-bit in order to receive a message.

    These lines would be deleted in the eCAN documentation