Other Parts Discussed in Thread: TCAN1042-Q1
Hi All,
Is it possible to interface the TMS320F28027F MCU with TCAN1042-Q1 to create a CAN interface with the TMS320F28027F device?
- Leo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
Is it possible to interface the TMS320F28027F MCU with TCAN1042-Q1 to create a CAN interface with the TMS320F28027F device?
- Leo
Hi Leo,
This TCAN chip acts as a CAN/CANFD transceiver, and needs to be used along with a device which has a CAN interface.
The F2802x family of devices does not have a CAN peripheral, and therefore it will not be able to interface.
However, the F2803x family & F2806xF families do have eCAN peripherals, and they will likely be able to interface to this TCAN transceiver to create a CAN node. Please note that the eCAN peripheral is designed to work with CAN networks (not the newer, higher datarate, CAN-FD). Because of this, and assuming that a standard CAN network is what is being implemented, there may be cheaper TI CAN transceivers to consider.
Thank you,
Brett