Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

generating pulses using TMS320F28335 c2000 series microcontroller.

Other Parts Discussed in Thread: TMS320F28335, CONTROLSUITE

Respected sir/ Madam

    I am doing project on inverters.I need to produce gate pulses.For that i am using TMS320f28335 micro controller. I tried with examples it self from Control suite 3.3. But after running the code in CCS5 version i didn't see any pulses at pin number 23(EPWM-1A).Could any one kindly help me on this.I tried for 2 month before. But this most requirement for my project.And i uploaded some pics.I observed that while running the code no EPWM  register is updated. I am not getting it briefly.

 I didn't observe changing values in EPWM 1A register.


From CRO i didn't get any pulses.It is constantly showing the 3.4V when i connected with PC.