Other Parts Discussed in Thread: TEST
Tool/software: Code Composer Studio
Hello all,
I am trying to make a SPI communication with Simulink and the F28M36. As you can imagine, it doesn't work. I have already made some code with Simulink to the card and everything works fine.
I only have trouble with SPI (till now). A strange thing is that the Simulink compiler works and deploy the "program" to the card (and there is nothing on the SPI pins). When I open the CCSv7 to see the generated code, I realize that there are some errors.
"spi.h", line 27: fatal error: cannot open source file "MW_SPI.h"
1 catastrophic error detected in the compilation of "MW_c28xx_board.c".
When I check on my computer, I don't have any MW_SPI.h.
Could you help me ?
Antoine