Hi,
Customer faced one issue about F28066 Tx (pin43). When ARM is powered with 3.3V, F28066 is not powered. The voltage of point A will be lower to 2.0V.
Customer wants to know the reason.
In customer's board, F28066 has the SCI connection with ARM. They are powered separately. Supply currents are high enough, more than 500mA.
When F28066 loses its power, the voltage of point A will be driven low to 2.0V. They tried to adjust the resistance from 3.3K to 10K. There's no improvement.
Thanks.
Br, Jordan