This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28027F: Serial interrupt

Part Number: TMS320F28027F

Tool/software: TI C/C++ Compiler

I am trying to run examplce code Example_2802xSci_FFDLB_int.c .  I changed the CPU frequency at top and added a condition to set baud rate at 115200 if CPU frequency is 60 MHZ. Real term still shows junk value.
Here is the example code with changes-

//#############################################################################
//
// File: f2802x_examples/scia_loopback_interrupts/Example_F2802xSci_FFDLB_int.c
//
// Title: F2802x Device SCI Digital Loop Back program.
//
// Group: C2000
// Target Device: TMS320F2802x
//
//! \addtogroup example_list
//! <h1>SCI Digital Loop Back with Interrupts</h1>
//!
//! This program is a SCI example that uses the internal loopback of
//! the peripheral. Both interrupts and the SCI FIFOs are used.
//!
//! A stream of data is sent and then compared to the recieved stream.
//!
//! The SCI-A sent data looks like this: \n
//! 00 01 \n
//! 01 02 \n
//! 02 03 \n
//! .... \n
//! FE FF \n
//! FF 00 \n
//! etc..
//!
//! The pattern is repeated forever.
//!
//! Watch Variables:
//! - sdataA - Data being sent
//! - rdataA - Data received
//! - rdata_pointA - Keep track of where we are in the datastream.
//! This is used to check the incoming data
//
// (C) Copyright 2012, Texas Instruments, Inc.
//#############################################################################
// $TI Release: PACKAGE NAME $
// $Release Date: PACKAGE RELEASE DATE $
//#############################################################################

#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#include <stdio.h>
#include <file.h>

#include "common/include/adc.h"
#include "common/include/clk.h"
#include "common/include/flash.h"
#include "common/include/gpio.h"
#include "common/include/pie.h"
#include "common/include/pll.h"
#include "common/include/sci.h"
#include "common/include/wdog.h"

#define CPU_FREQ 60E6 // Default = 40 MHz. Change to 50E6 for 50 MHz devices
#define LSPCLK_FREQ CPU_FREQ/4
#define SCI_FREQ 100E3
#define SCI_PRD (LSPCLK_FREQ/(SCI_FREQ*8))-1

// Prototype statements for functions found within this file.
__interrupt void sciaTxFifoIsr(void);
__interrupt void sciaRxFifoIsr(void);
__interrupt void scibTxFifoIsr(void);
__interrupt void scibRxFifoIsr(void);
void scia_init(void);
void scia_fifo_init(void);
void error(void);

// Global variables
uint16_t sdataA[2]; // Send data for SCI-A
uint16_t rdataA[2]; // Received data for SCI-A
uint16_t rdata_pointA; // Used for checking the received data

ADC_Handle myAdc;
CLK_Handle myClk;
FLASH_Handle myFlash;
GPIO_Handle myGpio;
PIE_Handle myPie;
SCI_Handle mySci;

void main(void)
{
uint16_t i;

CPU_Handle myCpu;
PLL_Handle myPll;
WDOG_Handle myWDog;

// Initialize all the handles needed for this application
myAdc = ADC_init((void *)ADC_BASE_ADDR, sizeof(ADC_Obj));
myClk = CLK_init((void *)CLK_BASE_ADDR, sizeof(CLK_Obj));
myCpu = CPU_init((void *)NULL, sizeof(CPU_Obj));
myFlash = FLASH_init((void *)FLASH_BASE_ADDR, sizeof(FLASH_Obj));
myGpio = GPIO_init((void *)GPIO_BASE_ADDR, sizeof(GPIO_Obj));
myPie = PIE_init((void *)PIE_BASE_ADDR, sizeof(PIE_Obj));
myPll = PLL_init((void *)PLL_BASE_ADDR, sizeof(PLL_Obj));
mySci = SCI_init((void *)SCIA_BASE_ADDR, sizeof(SCI_Obj));
myWDog = WDOG_init((void *)WDOG_BASE_ADDR, sizeof(WDOG_Obj));

// Perform basic system initialization
WDOG_disable(myWDog);
CLK_enableAdcClock(myClk);
(*Device_cal)();

//Select the internal oscillator 1 as the clock source
CLK_setOscSrc(myClk, CLK_OscSrc_Internal);

// Setup the PLL for x10 /2 which will yield 50Mhz = 10Mhz * 10 / 2
PLL_setup(myPll, PLL_Multiplier_12, PLL_DivideSelect_ClkIn_by_2);

// Disable the PIE and all interrupts
PIE_disable(myPie);
PIE_disableAllInts(myPie);
CPU_disableGlobalInts(myCpu);
CPU_clearIntFlags(myCpu);

// If running from flash copy RAM only functions to RAM
#ifdef _FLASH
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
#endif

// Initialize GPIO
GPIO_setPullUp(myGpio, GPIO_Number_28, GPIO_PullUp_Enable);
GPIO_setPullUp(myGpio, GPIO_Number_29, GPIO_PullUp_Disable);
GPIO_setQualification(myGpio, GPIO_Number_28, GPIO_Qual_ASync);
GPIO_setMode(myGpio, GPIO_Number_28, GPIO_28_Mode_SCIRXDA);
GPIO_setMode(myGpio, GPIO_Number_29, GPIO_29_Mode_SCITXDA);

// Setup a debug vector table and enable the PIE
PIE_setDebugIntVectorTable(myPie);
PIE_enable(myPie);

// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
EALLOW; // This is needed to write to EALLOW protected registers
// PieVectTable.SCIRXINTA = &sciaRxFifoIsr;
((PIE_Obj *)myPie)->SCIRXINTA = &sciaRxFifoIsr;
// PieVectTable.SCITXINTA = &sciaTxFifoIsr;
((PIE_Obj *)myPie)->SCITXINTA = &sciaTxFifoIsr;
EDIS; // This is needed to disable write to EALLOW protected registers

// Register interrupt handlers in the PIE vector table
PIE_registerPieIntHandler(myPie, PIE_GroupNumber_9, PIE_SubGroupNumber_1, (intVec_t)&sciaRxFifoIsr);
PIE_registerPieIntHandler(myPie, PIE_GroupNumber_9, PIE_SubGroupNumber_2, (intVec_t)&sciaTxFifoIsr);

scia_init(); // Init SCI-A
scia_fifo_init(); // Init SCI-A Fifos

// Init send data. After each transmission this data
// will be updated for the next transmission
for(i = 0; i<2; i++)
{
sdataA[i] = i;
}

rdata_pointA = sdataA[0];
// Enable interrupts required for this example
PIE_enableInt(myPie, PIE_GroupNumber_9, PIE_InterruptSource_SCIARX);
PIE_enableInt(myPie, PIE_GroupNumber_9, PIE_InterruptSource_SCIATX);

CPU_enableInt(myCpu, CPU_IntNumber_9);
CPU_enableGlobalInts(myCpu);

for(;;){
}

}

void error(void)
{
__asm(" ESTOP0"); // Test failed!! Stop!
for (;;){
}
}

__interrupt void sciaTxFifoIsr(void)
{
uint16_t i;
for(i=0; i< 2; i++) {
// Send data
SCI_putDataBlocking(mySci, sdataA[i]);
}

for(i=0; i< 2; i++) {
//Increment send data for next cycle
sdataA[i] = (sdataA[i]+1) & 0x00FF;
}

// Clear SCI Interrupt flag
SCI_clearTxFifoInt(mySci);

// Issue PIE ACK
PIE_clearInt(myPie, PIE_GroupNumber_9);

return;
}

__interrupt void sciaRxFifoIsr(void)
{
uint16_t i;

if(SCI_getRxFifoStatus(mySci) != SCI_FifoLevel_Empty){
for(i=0;i<2;i++) {
// Read data
rdataA[i] = SCI_getData(mySci);
}
for(i=0;i<2;i++) {
// Check received data
if(rdataA[i] != ( (rdata_pointA+i) & 0x00FF) )
error();
}

rdata_pointA = (rdata_pointA+1) & 0x00FF;
}

// Clear Overflow flag
SCI_clearRxFifoOvf(mySci);

// Clear Interrupt flag
SCI_clearRxFifoInt(mySci);

// Issue PIE ack
PIE_clearInt(myPie, PIE_GroupNumber_9);

return;
}

void scia_init()
{

CLK_enableSciaClock(myClk);

// 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
SCI_disableParity(mySci);
SCI_setNumStopBits(mySci, SCI_NumStopBits_One);
SCI_setCharLength(mySci, SCI_CharLength_8_Bits);

// enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
SCI_enableTx(mySci);
SCI_enableRx(mySci);
SCI_enableTxInt(mySci);
SCI_enableRxInt(mySci);

SCI_enableLoopBack(mySci);

// SCI BRR = LSPCLK/(SCI BAUDx8) - 1
#if (CPU_FRQ_60MHZ)
SCI_setBaudRate(mySci, (SCI_BaudRate_e)15);
#elif (CPU_FRQ_50MHZ)
SCI_setBaudRate(mySci, (SCI_BaudRate_e)15);
#endif

SCI_enable(mySci);

return;
}

void scia_fifo_init()
{

SCI_enableFifoEnh(mySci);
SCI_resetTxFifo(mySci);
SCI_clearTxFifoInt(mySci);
SCI_resetChannels(mySci);
SCI_setTxFifoIntLevel(mySci, SCI_FifoLevel_2_Words);
SCI_enableTxFifoInt(mySci);

SCI_resetRxFifo(mySci);
SCI_clearRxFifoInt(mySci);
SCI_setRxFifoIntLevel(mySci, SCI_FifoLevel_2_Words);
SCI_enableRxFifoInt(mySci);

return;
}


//===========================================================================
// No more.
//===========================================================================

  • I would recommended first hooking up a scope and measuring the baud rate while transmitting 0x55. Is the board transmitting at the correct baud?
  • SCi_echoback example code is working fine. So, it works perfectly at the predefined baud rate.
  • Echo back uses the same UART module for both transmit and receive. In other words, even if baud is set incorrectly, it'll still work because they are using the same baud rate generator.
  • Sarthak,

    You might need to double-check your baud settings (note they are the same for both CPU frequencies). From the above modified code:

    // SCI BRR = LSPCLK/(SCI BAUDx8) - 1
    #if (CPU_FRQ_60MHZ)
    SCI_setBaudRate(mySci, (SCI_BaudRate_e)15);
    #elif (CPU_FRQ_50MHZ)
    SCI_setBaudRate(mySci, (SCI_BaudRate_e)15);
    #endif

    - Ken
  • Sorry for teh late reply. Here is the update code. Cpu frequency is set to 50 MHz. To set baud rate at 9600 , BRR is 162 .

    //
    // Included Files
    //
    #include "DSP28x_Project.h" // Device Headerfile and Examples Include File
    #include <stdio.h>
    #include <file.h>

    #include "common/include/adc.h"
    #include "common/include/clk.h"
    #include "common/include/flash.h"
    #include "common/include/gpio.h"
    #include "common/include/pie.h"
    #include "common/include/pll.h"
    #include "common/include/sci.h"
    #include "common/include/wdog.h"

    //
    // Defines
    //

    //
    // Default = 40 MHz. Change to 50E6 for 50 MHz devices
    //
    #define CPU_FREQ 50E6
    #define LSPCLK_FREQ CPU_FREQ/4
    #define SCI_FREQ 9600
    #define SCI_PRD (LSPCLK_FREQ/(SCI_FREQ*8))-1

    //
    // Function Prototypes
    //
    __interrupt void sciaTxFifoIsr(void);
    __interrupt void sciaRxFifoIsr(void);
    __interrupt void scibTxFifoIsr(void);
    __interrupt void scibRxFifoIsr(void);
    void scia_init(void);
    void scia_fifo_init(void);
    void error(void);

    //
    // Globals
    //
    uint16_t sdataA[2]; // Send data for SCI-A
    uint16_t rdataA[2]; // Received data for SCI-A
    uint16_t rdata_pointA; // Used for checking the received data

    ADC_Handle myAdc;
    CLK_Handle myClk;
    FLASH_Handle myFlash;
    GPIO_Handle myGpio;
    PIE_Handle myPie;
    SCI_Handle mySci;

    //
    // Main
    //
    void main(void)
    {
    uint16_t i;

    CPU_Handle myCpu;
    PLL_Handle myPll;
    WDOG_Handle myWDog;

    //
    // Initialize all the handles needed for this application
    //
    myAdc = ADC_init((void *)ADC_BASE_ADDR, sizeof(ADC_Obj));
    myClk = CLK_init((void *)CLK_BASE_ADDR, sizeof(CLK_Obj));
    myCpu = CPU_init((void *)NULL, sizeof(CPU_Obj));
    myFlash = FLASH_init((void *)FLASH_BASE_ADDR, sizeof(FLASH_Obj));
    myGpio = GPIO_init((void *)GPIO_BASE_ADDR, sizeof(GPIO_Obj));
    myPie = PIE_init((void *)PIE_BASE_ADDR, sizeof(PIE_Obj));
    myPll = PLL_init((void *)PLL_BASE_ADDR, sizeof(PLL_Obj));
    mySci = SCI_init((void *)SCIA_BASE_ADDR, sizeof(SCI_Obj));
    myWDog = WDOG_init((void *)WDOG_BASE_ADDR, sizeof(WDOG_Obj));

    //
    // Perform basic system initialization
    //
    WDOG_disable(myWDog);
    CLK_enableAdcClock(myClk);
    (*Device_cal)();

    //
    // Select the internal oscillator 1 as the clock source
    //
    CLK_setOscSrc(myClk, CLK_OscSrc_Internal);

    //
    // Setup the PLL for x10 /2 which will yield 50Mhz = 10Mhz * 10 / 2
    //
    PLL_setup(myPll, PLL_Multiplier_10, PLL_DivideSelect_ClkIn_by_2);

    //
    // Disable the PIE and all interrupts
    //
    PIE_disable(myPie);
    PIE_disableAllInts(myPie);
    CPU_disableGlobalInts(myCpu);
    CPU_clearIntFlags(myCpu);

    //
    // If running from flash copy RAM only functions to RAM
    //
    #ifdef _FLASH
    memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
    #endif

    //
    // Initialize GPIO
    //
    GPIO_setPullUp(myGpio, GPIO_Number_28, GPIO_PullUp_Enable);
    GPIO_setPullUp(myGpio, GPIO_Number_29, GPIO_PullUp_Disable);
    GPIO_setQualification(myGpio, GPIO_Number_28, GPIO_Qual_ASync);
    GPIO_setMode(myGpio, GPIO_Number_28, GPIO_28_Mode_SCIRXDA);
    GPIO_setMode(myGpio, GPIO_Number_29, GPIO_29_Mode_SCITXDA);
    // GPIO_setMode(myGpio, GPIO_Number_18, GPIO_18_Mode_XCLKOUT);
    // CLK_setClkOutPreScaler(myClk, CLK_ClkOutPreScaler_SysClkOut_by_4);

    //
    // Setup a debug vector table and enable the PIE
    //
    PIE_setDebugIntVectorTable(myPie);
    PIE_enable(myPie);

    //
    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
    //
    EALLOW; // This is needed to write to EALLOW protected registers
    //PieVectTable.SCIRXINTA = &sciaRxFifoIsr;
    ((PIE_Obj *)myPie)->SCIRXINTA = &sciaRxFifoIsr;
    //PieVectTable.SCITXINTA = &sciaTxFifoIsr;
    ((PIE_Obj *)myPie)->SCITXINTA = &sciaTxFifoIsr;
    EDIS; // This is needed to disable write to EALLOW protected registers

    //
    // Register interrupt handlers in the PIE vector table
    //
    PIE_registerPieIntHandler(myPie, PIE_GroupNumber_9, PIE_SubGroupNumber_1,
    (intVec_t)&sciaRxFifoIsr);
    PIE_registerPieIntHandler(myPie, PIE_GroupNumber_9, PIE_SubGroupNumber_2,
    (intVec_t)&sciaTxFifoIsr);

    scia_init(); // Init SCI-A
    scia_fifo_init(); // Init SCI-A Fifos

    //
    // Init send data. After each transmission this data will be updated for
    // the next transmission
    //
    for(i = 0; i<2; i++)
    {
    sdataA[i] = i;
    }

    rdata_pointA = sdataA[0];

    //
    // Enable interrupts required for this example
    //
    PIE_enableInt(myPie, PIE_GroupNumber_9, PIE_InterruptSource_SCIARX);
    PIE_enableInt(myPie, PIE_GroupNumber_9, PIE_InterruptSource_SCIATX);

    CPU_enableInt(myCpu, CPU_IntNumber_9);
    CPU_enableGlobalInts(myCpu);

    for(;;)
    {

    }
    }

    //
    // error -
    //
    void error(void)
    {
    __asm(" ESTOP0"); // Test failed!! Stop!
    for (;;)
    {

    }
    }

    //
    // sciaTxFifoIsr -
    //
    __interrupt void
    sciaTxFifoIsr(void)
    {
    uint16_t i;
    for(i=0; i< 2; i++)
    {
    //
    // Send data
    //
    // SCI_putDataBlocking(mySci, sdataA[i]);
    }

    for(i=0; i< 2; i++)
    {
    //
    // Increment send data for next cycle
    //
    sdataA[i] = (sdataA[i]+1) & 0x00FF;
    }

    //
    // Clear SCI Interrupt flag
    //
    SCI_clearTxFifoInt(mySci);

    //
    // Issue PIE ACK
    //
    PIE_clearInt(myPie, PIE_GroupNumber_9);

    return;
    }

    //
    // sciaRxFifoIsr -
    //
    __interrupt void
    sciaRxFifoIsr(void)
    {
    uint16_t i;

    if(SCI_getRxFifoStatus(mySci) != SCI_FifoLevel_Empty)
    {
    for(i=0;i<2;i++)
    {
    //
    // Read data
    //
    rdataA[i] = SCI_getData(mySci);
    }

    for(i=0;i<2;i++)
    {
    //
    // Check received data
    //
    if(rdataA[i] != ( (rdata_pointA+i) & 0x00FF) )
    {
    // error();
    }
    }

    rdata_pointA = (rdata_pointA+1) & 0x00FF;
    }

    //
    // Clear Overflow flag
    //
    SCI_clearRxFifoOvf(mySci);

    //
    // Clear Interrupt flag
    //
    SCI_clearRxFifoInt(mySci);

    //
    // Issue PIE ack
    //
    PIE_clearInt(myPie, PIE_GroupNumber_9);

    return;
    }

    //
    // scia_init -
    //
    void
    scia_init()
    {
    CLK_enableSciaClock(myClk);

    //
    // 1 stop bit, No loopback, No parity, 8 char bits, async mode
    // idle-line protocol
    //
    SCI_disableParity(mySci);
    SCI_setNumStopBits(mySci, SCI_NumStopBits_One);
    SCI_setCharLength(mySci, SCI_CharLength_8_Bits);

    //
    // enable TX, RX, internal SCICLK, Disable RX ERR, SLEEP, TXWAKE
    //
    SCI_enableTx(mySci);
    SCI_enableRx(mySci);
    SCI_enableTxInt(mySci);
    SCI_enableRxInt(mySci);

    SCI_enableLoopBack(mySci);

    //SCI BRR = LSPCLK/(SCI BAUDx8) - 1
    #if (CPU_FRQ_50MHZ)
    SCI_setBaudRate(mySci, (SCI_BaudRate_e)162);
    #elif (CPU_FRQ_40MHZ)
    SCI_setBaudRate(mySci, (SCI_BaudRate_e)129);
    #endif

    SCI_enable(mySci);

    return;
    }

    //
    // scia_fifo_init -
    //
    void
    scia_fifo_init()
    {
    SCI_enableFifoEnh(mySci);
    SCI_resetTxFifo(mySci);
    SCI_clearTxFifoInt(mySci);
    SCI_resetChannels(mySci);
    SCI_setTxFifoIntLevel(mySci, SCI_FifoLevel_2_Words);
    SCI_enableTxFifoInt(mySci);

    SCI_resetRxFifo(mySci);
    SCI_clearRxFifoInt(mySci);
    SCI_setRxFifoIntLevel(mySci, SCI_FifoLevel_2_Words);
    SCI_enableRxFifoInt(mySci);

    return;
    }

    //
    // End of File
    //

  • Sarthak,

    You only sent me your updated code, but did not provide any other information about the results. Does your code work at the default frequency of 40 MHz? Can you get the unmodified original code to work?

    - Ken
  • Ken,
    With any frequency , I can print when I am sending commands through Tx isr but nothing happens when I send commands through putty. Do I have to make some changes to receive commands through serial instead if tx Isr.
  • When I send commands through puttuy, tx line blinks instead of rx line. How can this be solved?
  • Sarthak,

    Does the original unmodified program work? I want to find out if the issue is the code or something else (putty).

    - Ken
  • Sarthak,

    It's been a few week since we have heard from you last. Therefore, we are assuming you were able to resolve your issue. If this isn’t the case, please reject this resolution or reply to this thread. If this thread locks, please make a new thread describing the current status of your issue. Thank you.

    - Ken