Part Number: DRV8302-HC-C2-KIT
Other Parts Discussed in Thread: DRV8301, DRV8302, DRV8312
Hello,
I am using the DRV8302-HC-C2-KIT for a senior design project. I am using it to control a BLDC motor for a small car. In order to use the motor from the board I am also using an analog foot throttle. I was able to have code flashed onto the board using code composer studio and get the motor to run fine. Although I am having trouble finding exactly what pin that I need to use on the board for my analog signal foot throttle. Not very familiar with these types of applications and need advice on this issue.
I have attached the code that I am using.
My foot throttle is a three wire connection - black (ground) red (power) green (speed signal) Input signal: 5V Output: 0.8-4.2V
Thank you for the help,
Blake Fredieu
/* ==============================================================================
System Name: DRV83xx EVM Integrated Flash Image for use with GUI
File Name: BLDC_Int_GUI_DRV83xx.c
Description: Primary system file for the Implementation of BEMF Integration with
GUI control
Originator: Digital control systems Group - Texas Instruments
=====================================================================================
History:
-------------------------------------------------------------------------------------
xx Aug 2011: Jon Warriner
================================================================================= */
// Include header files used in the main function
#include "PeripheralHeaderIncludes.h"
#include "BLDC_Int_GUI_DRV83xx-Settings.h"
#include "IQmathLib.h"
#include "BLDC_Int_GUI_DRV83xx.h"
#include "Graph_Data.h"
#include "Commros_user.h"
#include <math.h>
#define REFVOLTS 0.85
// Prototype statements for functions found within this file.
interrupt void MainISR(void);
void DeviceInit();
void MemCopy();
void InitFlash();
void Gui_DBUFF_init();
// State Machine function prototypes
//------------------------------------
// Alpha states
void A0(void); //state A0
void B0(void); //state B0
void C0(void); //state C0
// A branch states
void A1(void); //state A1
void A2(void); //state A2
void A3(void); //state A3
// B branch states
void B1(void); //state B1
void B2(void); //state B2
void B3(void); //state B3
// C branch states
void C1(void); //state C1
void C2(void); //state C2
void C3(void); //state C3
// Variable declarations
void (*Alpha_State_Ptr)(void); // Base States pointer
void (*A_Task_Ptr)(void); // State pointer A branch
void (*B_Task_Ptr)(void); // State pointer B branch
void (*C_Task_Ptr)(void); // State pointer C branch
// Used for running BackGround in flash, and ISR in RAM
extern Uint16 *RamfuncsLoadStart, *RamfuncsLoadEnd, *RamfuncsRunStart;
//GUI variables
//Want to place these in their own memory section that won't move around as
//non-gui variables are added/deleted.
#pragma DATA_SECTION(Gui,"GUIVARS");
struct GUI_VARS Gui;
// Global variables used in this system (but not by the GUI)
// Define the electrical motor parametes
float RS; // Stator resistance (ohm)
float RR; // Rotor resistance (ohm)
float LS; // Stator inductance (H)
float LR; // Rotor inductance (H)
float LM; // Magnatizing inductance (H)
// Define the base quantites for PU system conversion
float BASE_VOLTAGE; // Base peak phase voltage (volt)
float BASE_CURRENT; // Base peak phase current (amp)
float32 T; // Samping period (sec)
_iq BemfA = 0;
_iq BemfB = 0;
_iq BemfC = 0;
_iq IDC_offset = _IQ(0.5);
_iq IA_offset = _IQ(0.5);
_iq IRef=_IQ(0.0); // Id reference (pu)
_iq SpeedRef=_IQ(0.0); // Speed reference (pu)
_iq cal_filt_gain;
_iq spd_filt_gain;
_iq DfuncRun;
AdcRegs.ADCSOC7CTL.bit.CHSEL = 4;
AdcRegs.ADCSOC7CTL.bit.TRIGSEL = 5;
AdcRegs.ADCSOC7CTL.bit.ACQPS = 6;
Uint32 VirtualTimer = 0;
Uint32 IsrTicker = 0;
Uint32 CmtnPeriodTarget;
Uint32 CmtnPeriodSetpt;
int32 RAMP_START_RATE;
int32 RAMP_END_RATE;
Uint16 CALIBRATE_FLAG = 1;
Uint16 CALIBRATE_TIME = 0x07FF; //give the calibration filters about 100ms (~10tc) to settle
Uint16 BackTicker = 0;
Uint16 PreviousState;
Uint16 SpeedLoopFlag = FALSE;
Uint16 RunBLDC_Int=0;
Uint16 ISR_FREQUENCY=20; // Define the ISR frequency (kHz)
Uint16 PWM_FREQUENCY=20; // Define the ISR frequency (kHz)
Uint16 control_mode = 0;
int16 VTimer0[4]; // Virtual Timers slaved off CPU Timer 0 (A events)
int16 VTimer1[4]; // Virtual Timers slaved off CPU Timer 1 (B events)
int16 VTimer2[4]; // Virtual Timers slaved off CPU Timer 2 (C events)
int16 K_VdcBus = 6632;
int16 i; // common use incrementer
_iq DlogCh1 = 0;
_iq DlogCh2 = 0;
_iq DlogCh3 = 0;
int16 LedBlinkCnt=50;
int16 DlogCurrElementIndex=0;
int16 PwmDacCh1 = 0;
int16 PwmDacCh2 = 0;
int16 PwmDacCh3 = 0;
#if defined(DRV8301) || defined(DRV8302)
int16 PwmDacCh4 = 0;
#endif
_iq *dlogptr1;
_iq *dlogptr2;
_iq *dlogptr3;
// Instance PID regulator to regulate the DC-bus current and speed
PID_GRANDO_CONTROLLER pid1_idc = {PID_TERM_DEFAULTS,PID_PARAM_DEFAULTS,PID_DATA_DEFAULTS};
PID_GRANDO_CONTROLLER pid1_spd = {PID_TERM_DEFAULTS,PID_PARAM_DEFAULTS,PID_DATA_DEFAULTS};
// Instance a PWM driver instance
PWM_CNTL pwmcntl1 = PWM_CNTL_DEFAULTS;
// Instance a PWM DAC driver instance
PWMDAC pwmdac1 = PWMDAC_DEFAULTS;
// Instance a ramp controller to smoothly ramp the frequency
RMPCNTL rc1 = RMPCNTL_DEFAULTS;
// Instance a RAMP3 Module
RMP3 rmp3 = RMP3_DEFAULTS;
// Instance a MOD6 Module
MOD6CNTDIR mod_dir1 = MOD6CNTDIR_DEFAULTS;
// Instance a IMPULSE Module
IMPULSE impl1 = IMPULSE_DEFAULTS;
//Instance an InstaSPIN_BLDC Module
INSTASPIN_BLDC InstaSPIN_BLDC1 = INSTASPIN_BLDC_DEFAULTS;
// Instance a SPEED_PR Module
SPEED_MEAS_CAP speed1 = SPEED_MEAS_CAP_DEFAULTS;
// Create an instance of DATALOG Module
struct GRAPH_DATA gdata;
#ifdef DRV8301
union DRV8301_STATUS_REG_1 DRV8301_stat_reg1;
union DRV8301_STATUS_REG_2 DRV8301_stat_reg2;
union DRV8301_CONTROL_REG_1 DRV8301_cntrl_reg1;
union DRV8301_CONTROL_REG_2 DRV8301_cntrl_reg2;
Uint16 read_drv_status = 0;
#endif
Uint32 BemfTrigCnt = 0;
Uint32 BemfLastTrigCnt = 0;
Uint16 GoodTrigCnt = 0;
Uint16 ClosedCommutationFlag = 0;
Uint16 GoodTrigCntTrip = 20;
void main(void)
{
DeviceInit(); // Device Life support & GPIO
// Only used if running from FLASH
// Note that the variable FLASH is defined by the compiler
#ifdef FLASH
// Copy time critical code and Flash setup code to RAM
// The RamfuncsLoadStart, RamfuncsLoadEnd, and RamfuncsRunStart
// symbols are created by the linker. Refer to the linker files.
MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
// Call Flash Initialization to setup flash waitstates
// This function must reside in RAM
InitFlash(); // Call the flash wrapper init function
#endif //(FLASH)
// Tasks State-machine init
Alpha_State_Ptr = &A0;
A_Task_Ptr = &A1;
B_Task_Ptr = &B1;
// C_Task_Ptr = &C1;
// Configure CPU-Timer 2 to interrupt every ISR Period:
// 60MHz CPU Freq, ISR Period (in uSeconds)
// This function is found in DSP280x_CpuTimers.c
//jpw InitCpuTimers();
//jpw ConfigCpuTimer(&CpuTimer0, 60, SYSTEM_FREQUENCY*10/ISR_FREQUENCY);
//jpw StartCpuTimer0();
#ifdef DRV8301
// Initialize SPI for communication to the DRV8301
DRV8301_SPI_Init(&SpibRegs);
#endif
// Timing sync for background loops
// Timer period definitions found in device specific PeripheralHeaderIncludes.h
// CpuTimer0Regs.PRD.all = mSec1; //
CpuTimer1Regs.PRD.all = mSec1; // A tasks
CpuTimer2Regs.PRD.all = mSec5; // B tasks
Gui.Ref = _IQ(0.0); //originally 0.3 //written by the Reference knob in the GUI
Gui.CurrentDisplay = _IQ(0.0); //read by the GUI to display motor current
Gui.DfuncStartup = _IQ(0.1); //written by the GUI to set startup duty cycle
#if defined(DRV8312)
Gui.CurrentStartup = _IQ(0.1); //written by the GUI to set startup duty cycle
#endif
#if defined(DRV8301) || defined(DRV8302)
Gui.CurrentStartup = _IQ(0.02); //written by the GUI to set startup duty cycle
#endif
Gui.Threshold = _IQ(2); //originally .4 //written by the GUI to set Integration threshold
#if defined(DRV8312)
Gui.Current_Kp = _IQ(0.1);
#endif
#if defined(DRV8301) || defined(DRV8302)
Gui.Current_Kp = _IQ(1.0);
#endif
Gui.Velocity_Kp = _IQ(0.5);
Gui.I_max = _IQ(0.95);
Gui.RampUpTime = 25;
Gui.CommErrorMax = 1.0;
Gui.TripCnt = 3;
Gui.AdvancedStartup = 0;
Gui.SpeedRPM = 0; //read by the GUI to display motor speed in RPM
Gui.BEGIN_START_RPM = 50; //written by the GUI to set start speed of ramp up controller
Gui.END_START_RPM = 100; //written by the GUI to set end speed of ramp up controller
Gui.current_mode = 0;
Gui.velocity_mode = 0;
Gui.ResetFault = 0;
Gui.POLES = 48; // Number of poles originally 8
Gui.Current_Ki = 20;
Gui.Velocity_Ki = 3;
Gui.Prescaler = 1;
Gui.OverVoltage=0;
Gui.DRVFaultFlag=0;
Gui.DRVOTWFlag = 0;
Gui.EnableFlag = TRUE; //originally FALSE
Gui.VdcBus = 0;
#if defined(DRV8312)
Gui.Max_VDC = 2880;
Gui.Min_VDC = 1920;
#endif
#if defined(DRV8301) || defined(DRV8302)
Gui.Max_VDC = 6000;
Gui.Min_VDC = 800;
#endif
// Reassign ISRs.
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.ADCINT1 = &MainISR;
EDIS; // This is needed to disable write to EALLOW protected registers
// Enable PIE group 1 interrupt 1 for ADCINT1
PieCtrlRegs.PIEIER1.all = M_INT1;
InitCommros();
// Define the base quantites for PU system conversion
BASE_VOLTAGE = 66.32; // Base peak phase voltage (volt), maximum measurable DC Bus
#if defined(DRV8312)
BASE_CURRENT = 8.6; // Base peak phase current (amp)
#endif
#if defined(DRV8301) || defined(DRV8302)
//options for BASE_CURRENT based on DRV830x current-sense amplifier gain setting
//NOTE: DRV8302 can only be set to gain of 10 or 40
BASE_CURRENT = 82.5; // Base peak phase current (amp) , maximum measurable peak current (with DRV830x gain set to 10)
// BASE_CURRENT = 41.25; // Base peak phase current (amp) , maximum measurable peak current (with DRV830x gain set to 20)
// BASE_CURRENT = 20.625; // Base peak phase current (amp) , maximum measurable peak current (with DRV830x gain set to 40)
// BASE_CURRENT = 10.3125; // Base peak phase current (amp) , maximum measurable peak current (with DRV830x gain set to 80)
#endif
Gui.BASE_FREQ = 200; // Base electrical frequency (Hz)
// Define the ISR frequency (kHz)
ISR_FREQUENCY=20;
PWM_FREQUENCY=ISR_FREQUENCY;
T = 0.001/ISR_FREQUENCY; // Samping period (sec), see parameter.h
// Initialize the PWM control module
pwmcntl1.PWMprd = SYSTEM_FREQUENCY*1000000*T/2; // Set the pwm period for this example
PWM_CNTL_INIT_MACRO(pwmcntl1)
PWM_CNTL_MACRO(pwmcntl1)
// Initialize PWMDAC module
pwmdac1.PeriodMax = 500; // 3000->10kHz, 1500->20kHz, 1000-> 30kHz, 500->60kHz
pwmdac1.PwmDacInPointer0 = &PwmDacCh1;
pwmdac1.PwmDacInPointer1 = &PwmDacCh2;
pwmdac1.PwmDacInPointer2 = &PwmDacCh3;
#if defined(DRV8301) || defined(DRV8302)
pwmdac1.PwmDacInPointer3 = &PwmDacCh4;
#endif
PWMDAC_INIT_MACRO(pwmdac1)
RAMP_START_RATE = (PWM_FREQUENCY*1000)*60.0/Gui.BEGIN_START_RPM/COMMUTATES_PER_E_REV/(Gui.POLES/2.0);
RAMP_END_RATE = (PWM_FREQUENCY*1000)*60.0/Gui.END_START_RPM/COMMUTATES_PER_E_REV/(Gui.POLES/2.0);
CmtnPeriodTarget = RAMP_END_RATE;
CmtnPeriodSetpt = RAMP_START_RATE;
// Initialize DATALOG module
gdata.ch1_ptr = &DlogCh1;
gdata.ch2_ptr = &DlogCh2;
gdata.ch3_ptr = &DlogCh3;
gdata.trig_value = 1;
gdata.size = 0x100;
gdata.prescalar = Gui.Prescaler;
gdata.holdoff = 10000;
Graph_Data_Init(&gdata);
dlogptr1=DLOG_4CH_buff1;
dlogptr2=DLOG_4CH_buff2;
dlogptr3=DLOG_4CH_buff3;
// Initialize ADC module (F2803XIDC_VEMF.H)
ADC_MACRO_INIT()
// Initialize the SPEED_PR module
speed1.InputSelect = 0;
speed1.BaseRpm = 120*(Gui.BASE_FREQ/Gui.POLES);
speed1.SpeedScaler = (Uint32)(ISR_FREQUENCY/(1*(float32)Gui.BASE_FREQ*0.001));
// Initialize RMPCNTL module
rc1.RampDelayMax = 1;
rc1.RampLowLimit = _IQ(-1.0);
rc1.RampHighLimit = _IQ(1.0);
// Initialize RMP3 module
rmp3.DesiredInput = CmtnPeriodTarget;
rmp3.Ramp3Delay = (Uint32)(((float32)Gui.RampUpTime * 0.001)/((float32)(CmtnPeriodSetpt - CmtnPeriodTarget) * T));
rmp3.Out = CmtnPeriodSetpt;
rmp3.Ramp3Min = CmtnPeriodTarget;
//Initialize the INSTASPIN_BLDC module
InstaSPIN_BLDC1.VaOffset = 0;
InstaSPIN_BLDC1.VbOffset = 0;
InstaSPIN_BLDC1.VcOffset = 0;
InstaSPIN_BLDC1.Int_Threshold = Gui.Threshold;
// Initialize the PID_GRANDO_CONTROLLER module for dc-bus current
pid1_idc.param.Kp = Gui.Current_Kp;
pid1_idc.param.Kr = _IQ(1.0);
pid1_idc.param.Ki = _IQ(T * (float32)Gui.Current_Ki);
pid1_idc.param.Kd = _IQ(0/T);
pid1_idc.param.Km = _IQ(1.0);
pid1_idc.param.Umax = _IQ(0.95);
pid1_idc.param.Umin = _IQ(-0.95);
// Initialize the PID_GRANDO_CONTROLLER module for Speed
pid1_spd.param.Kp = Gui.Velocity_Kp;
pid1_spd.param.Kr = _IQ(1.0);
pid1_spd.param.Ki = _IQ(T * (float32)Gui.Velocity_Ki);
pid1_spd.param.Kd = _IQ(0/T);
pid1_spd.param.Km = _IQ(1.0);
pid1_spd.param.Umax = Gui.I_max;
pid1_spd.param.Umin = -Gui.I_max;
// Initialize the current offset calibration filter
cal_filt_gain = _IQ(T/(T+TC_CAL));
// Initialize the current offset calibration filter
spd_filt_gain = _IQ(T/(T+TC_SPD));
// Enable CPU INT1 for ADCINT1:
IER |= M_INT1;
// Enable global Interrupts and higher priority real-time debug events:
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
// IDLE loop. Just sit and loop forever:
for(;;) //infinite loop
{
// State machine entry & exit point
//===========================================================
(*Alpha_State_Ptr)(); // jump to an Alpha state (A0,B0,...)
//===========================================================
ServiceRoutine(&commros);
//try to detect and reset any SCI errors
//Specifically recover from a break detect that
//results when the USB cable is plugged in.
//The FTDI chip spews some long pulses on its
//Tx pin at power-up. If C2000 is running when
//this happens it triggers SCI break detect.
if(SciaRegs.SCIRXST.bit.RXERROR)
{
GpioDataRegs.GPACLEAR.bit.GPIO31 = 1;
SciaRegs.SCICTL1.bit.SWRESET = 0;
SciaRegs.SCICTL1.bit.SWRESET = 1;
}
else
{
GpioDataRegs.GPASET.bit.GPIO31 = 1;
}
// Update current and velocity loop PI gains from GUI
pid1_idc.param.Kp = Gui.Current_Kp;
pid1_idc.param.Ki = _IQ(T * (float32)Gui.Current_Ki);
pid1_spd.param.Kp = Gui.Velocity_Kp;
pid1_spd.param.Ki = _IQ(T * (float32)Gui.Velocity_Ki);
gdata.prescalar = Gui.Prescaler;
GoodTrigCntTrip = (Uint16)(((Gui.CommErrorMax / T) * 0.001) + 0.5);
#ifdef DRV8301
//read the status registers from the DRV8301
if(read_drv_status)
{
DRV8301_stat_reg1.all = DRV8301_SPI_Read(&SpibRegs,STAT_REG_1_ADDR);
DRV8301_stat_reg2.all = DRV8301_SPI_Read(&SpibRegs,STAT_REG_2_ADDR);
read_drv_status = 0;
}
#endif
}
} //END MAIN CODE
//=================================================================================
// STATE-MACHINE SEQUENCING AND SYNCRONIZATION FOR SLOW BACKGROUND TASKS
//=================================================================================
//--------------------------------- FRAMEWORK -------------------------------------
void A0(void)
{
// loop rate synchronizer for A-tasks
if(CpuTimer1Regs.TCR.bit.TIF == 1)
{
CpuTimer1Regs.TCR.bit.TIF = 1; // clear flag
//-----------------------------------------------------------
(*A_Task_Ptr)(); // jump to an A Task (A1,A2,A3,...)
//-----------------------------------------------------------
VTimer0[0]++; // virtual timer 0, instance 0 (spare)
}
Alpha_State_Ptr = &B0; // Comment out to allow only A tasks
}
void B0(void)
{
// loop rate synchronizer for B-tasks
if(CpuTimer2Regs.TCR.bit.TIF == 1)
{
CpuTimer2Regs.TCR.bit.TIF = 1; // clear flag
//-----------------------------------------------------------
(*B_Task_Ptr)(); // jump to a B Task (B1,B2,B3,...)
//-----------------------------------------------------------
VTimer1[0]++; // virtual timer 1, instance 0 (spare)
}
Alpha_State_Ptr = &A0; // Allow C state tasks
}
//=================================================================================
// A - TASKS (executed in every 1 msec)
//=================================================================================
//--------------------------------------------------------
void A1(void) // Used to enable disable PWM's for the inverter
//--------------------------------------------------------
{
if(Gui.EnableFlag==FALSE)
{
RunBLDC_Int=0;
//shut down all PWMs
#if defined (DRV8312)
PHASE_A_OFF;
PHASE_B_OFF;
PHASE_C_OFF;
#endif
#if defined(DRV8301) || defined(DRV8302)
//de-assert the DRV830x EN_GATE pin
GpioDataRegs.GPBCLEAR.bit.GPIO39 = 1;
#endif
EPwm1Regs.CMPA.half.CMPA=0; // PWM 1A - PhaseA
EPwm2Regs.CMPA.half.CMPA=0; // PWM 2A - PhaseB
EPwm3Regs.CMPA.half.CMPA=0; // PWM 3A - PhaseC
if(Gui.ResetFault == 1)
{
#if defined (DRV8312)
//reset the DRV chip
GpioDataRegs.GPACLEAR.bit.GPIO1 = 1;
GpioDataRegs.GPACLEAR.bit.GPIO3 = 1;
GpioDataRegs.GPACLEAR.bit.GPIO5 = 1;
#endif
#if defined(DRV8301) || defined(DRV8302)
//de-assert the DRV830x EN_GATE pin
GpioDataRegs.GPBCLEAR.bit.GPIO39 = 1;
#endif
Gui.ResetFault = 2;
}
else if(Gui.ResetFault == 2)
{
//reset the trip zone
EALLOW;
EPwm1Regs.TZCLR.bit.OST=1;
EPwm2Regs.TZCLR.bit.OST=1;
EPwm3Regs.TZCLR.bit.OST=1;
EDIS;
Gui.ResetFault = 0;
Gui.DRVFaultFlag = 0;
}
//zero all displayed variables when disabled
Gui.SpeedRPM = 0;
speed1.SpeedRpm = 0;
speed1.Speed = 0;
Gui.CurrentDisplay = 0;
CALIBRATE_FLAG = 1;
InstaSPIN_BLDC1.VaOffset = 0;
InstaSPIN_BLDC1.VbOffset = 0;
InstaSPIN_BLDC1.VcOffset = 0;
IDC_offset = _IQ(0.5);
SpeedLoopFlag=FALSE;
}
// if motor type is not defined
if((Gui.EnableFlag == TRUE) && (RunBLDC_Int == FALSE))
{
// Read GUI_SpeedRef Only when you have enabled the motor
SpeedRef = Gui.Ref;
if((RunBLDC_Int == 0) && (Gui.DRVFaultFlag == 0))
{
#if defined(DRV8301) || defined(DRV8302)
//assert the DRV830x EN_GATE pin
GpioDataRegs.GPBSET.bit.GPIO39 = 1;
DELAY_US(50000); //delay to allow DRV830x supplies to ramp up
#ifdef DRV8301
DRV8301_cntrl_reg1.bit.GATE_CURRENT = 0; // full current 1.7A
// DRV8301_cntrl_reg1.bit.GATE_CURRENT = 1; // med current 0.7A
// DRV8301_cntrl_reg1.bit.GATE_CURRENT = 2; // min current 0.25A
DRV8301_cntrl_reg1.bit.GATE_RESET = 0; // Normal Mode
DRV8301_cntrl_reg1.bit.PWM_MODE = 0; // six independant PWMs
// DRV8301_cntrl_reg1.bit.OC_MODE = 0; // current limiting when OC detected
DRV8301_cntrl_reg1.bit.OC_MODE = 1; // latched OC shutdown
// DRV8301_cntrl_reg1.bit.OC_MODE = 2; // Report on OCTWn pin and SPI reg only, no shut-down
// DRV8301_cntrl_reg1.bit.OC_MODE = 3; // OC protection disabled
// DRV8301_cntrl_reg1.bit.OC_ADJ_SET = 0; // OC @ Vds=0.060V
// DRV8301_cntrl_reg1.bit.OC_ADJ_SET = 4; // OC @ Vds=0.097V
// DRV8301_cntrl_reg1.bit.OC_ADJ_SET = 6; // OC @ Vds=0.123V
// DRV8301_cntrl_reg1.bit.OC_ADJ_SET = 9; // OC @ Vds=0.175V
DRV8301_cntrl_reg1.bit.OC_ADJ_SET = 15; // OC @ Vds=0.358V
// DRV8301_cntrl_reg1.bit.OC_ADJ_SET = 16; // OC @ Vds=0.403V
// DRV8301_cntrl_reg1.bit.OC_ADJ_SET = 17; // OC @ Vds=0.454V
// DRV8301_cntrl_reg1.bit.OC_ADJ_SET = 18; // OC @ Vds=0.511V
DRV8301_cntrl_reg1.bit.Reserved = 0;
// DRV8301_cntrl_reg2.bit.OCTW_SET = 0; // report OT and OC
DRV8301_cntrl_reg2.bit.OCTW_SET = 1; // report OT only
DRV8301_cntrl_reg2.bit.GAIN = 0; // CS amplifier gain = 10
// DRV8301_cntrl_reg2.bit.GAIN = 1; // CS amplifier gain = 20
// DRV8301_cntrl_reg2.bit.GAIN = 2; // CS amplifier gain = 40
// DRV8301_cntrl_reg2.bit.GAIN = 3; // CS amplifier gain = 80
DRV8301_cntrl_reg2.bit.DC_CAL_CH1 = 0; // not in CS calibrate mode
DRV8301_cntrl_reg2.bit.DC_CAL_CH2 = 0; // not in CS calibrate mode
DRV8301_cntrl_reg2.bit.OC_TOFF = 0; // normal mode
DRV8301_cntrl_reg2.bit.Reserved = 0;
//write to DRV8301 control register 1, returns status register 1
DRV8301_stat_reg1.all = DRV8301_SPI_Write(&SpibRegs,CNTRL_REG_1_ADDR,DRV8301_cntrl_reg1.all);
//write to DRV8301 control register 2, returns status register 1
DRV8301_stat_reg1.all = DRV8301_SPI_Write(&SpibRegs,CNTRL_REG_2_ADDR,DRV8301_cntrl_reg2.all);
#endif
#endif
// Define the base quantites for PU system conversion
BASE_VOLTAGE = 66.32; // Base peak phase voltage (volt), maximum measurable DC Bus
#if defined(DRV8312)
BASE_CURRENT = 8.6; // Base peak phase current (amp)
#endif
#if defined(DRV8301) || defined(DRV8302)
//options for BASE_CURRENT based on DRV830x current-sense amplifier gain setting
//NOTE: DRV8302 can only be set to gain of 10 or 40
BASE_CURRENT = 82.5; // Base peak phase current (amp) , maximum measurable peak current (with DRV830x gain set to 10)
// BASE_CURRENT = 41.25; // Base peak phase current (amp) , maximum measurable peak current (with DRV830x gain set to 20)
// BASE_CURRENT = 20.625; // Base peak phase current (amp) , maximum measurable peak current (with DRV830x gain set to 40)
// BASE_CURRENT = 10.3125; // Base peak phase current (amp) , maximum measurable peak current (with DRV830x gain set to 80)
#endif
// Define the ISR frequency (kHz)
ISR_FREQUENCY=20;
T = 0.001/ISR_FREQUENCY; // Samping period (sec), see parameter.h
speed1.InputSelect = 0;
speed1.BaseRpm = 120*(Gui.BASE_FREQ/Gui.POLES);
speed1.SpeedScaler = (Uint32)(ISR_FREQUENCY/(1*(float32)Gui.BASE_FREQ*0.001));
speed1.InputSelect = 0;
speed1.NewTimeStamp = 0;
speed1.OldTimeStamp = 0;
speed1.EventPeriod = 0;
speed1.Speed = 0;
VirtualTimer = 0;
rc1.EqualFlag = 0;
rc1.RampDelayCount = 0;
rc1.TargetValue = 0;
//The speed at the end of the ramp should always be greater than the speed at the beginning of the ramp
//If the GUI entries violate this use
//BEGIN_START_RPM = 50
//BEGIN_END_RPM = 100
if(Gui.END_START_RPM > Gui.BEGIN_START_RPM)
{
RAMP_START_RATE = (PWM_FREQUENCY*1000)*60.0/Gui.BEGIN_START_RPM/COMMUTATES_PER_E_REV/(Gui.POLES/2.0);
RAMP_END_RATE = (PWM_FREQUENCY*1000)*60.0/Gui.END_START_RPM/COMMUTATES_PER_E_REV/(Gui.POLES/2.0);
}
else
{
RAMP_START_RATE = (PWM_FREQUENCY*1000)*60.0/50/COMMUTATES_PER_E_REV/(Gui.POLES/2.0);
RAMP_END_RATE = (PWM_FREQUENCY*1000)*60.0/100/COMMUTATES_PER_E_REV/(Gui.POLES/2.0);
}
CmtnPeriodTarget = RAMP_END_RATE;
CmtnPeriodSetpt = RAMP_START_RATE;
rmp3.Ramp3Delay = (Uint32)(((float32)Gui.RampUpTime * 0.001)/((float32)(CmtnPeriodSetpt - CmtnPeriodTarget) * T));
rmp3.DesiredInput = CmtnPeriodTarget;
rmp3.Out = CmtnPeriodSetpt;
rmp3.Ramp3Min = CmtnPeriodTarget;
rmp3.Ramp3DelayCount = 0;
rmp3.Ramp3DoneFlag = 0;
impl1.Counter = 0;
impl1.Out = 0;
mod_dir1.Counter = 0;
SpeedLoopFlag = FALSE;
pid1_idc.data.d1 = 0;
pid1_idc.data.d2 = 0;
pid1_idc.data.i1 = 0;
pid1_idc.data.ud = 0;
pid1_idc.data.ui = 0;
pid1_idc.data.up = 0;
pid1_idc.data.v1 = 0;
pid1_idc.data.w1 = 0;
pid1_idc.term.Out = 0;
pid1_spd.data.d1 = 0;
pid1_spd.data.d2 = 0;
pid1_spd.data.i1 = 0;
pid1_spd.data.ud = 0;
pid1_spd.data.ui = 0;
pid1_spd.data.up = 0;
pid1_spd.data.v1 = 0;
pid1_spd.data.w1 = 0;
pid1_spd.term.Out = 0;
pid1_spd.param.Umax = Gui.I_max;
pid1_spd.param.Umin = -Gui.I_max;
DfuncRun = Gui.DfuncStartup;
BemfTrigCnt = 0;
BemfLastTrigCnt = 0;
GoodTrigCnt = 0;
ClosedCommutationFlag = 0;
InstaSPIN_BLDC1.V_int = 0;
//set control_mode based on check box settings from GUI
//VOLTAGE 0 //open-loop volage mode only
//CURRENT 1 //closed-loop current control
//VELOCITY 2 //closed-loop velocity control
//CASCADE 3 //cascaded closed-loop velocity->current control
//velocity loop check box writes either 0 (disabled) or 2 (enabled)
//current loop check box writes either 0 (disabled) or 1 (enabled)
control_mode = Gui.velocity_mode + Gui.current_mode;
RunBLDC_Int=1;
EALLOW;
EPwm1Regs.TZCLR.bit.OST=1;
EPwm2Regs.TZCLR.bit.OST=1;
EPwm3Regs.TZCLR.bit.OST=1;
EDIS;
}
}
//-------------------
//the next time CpuTimer0 'counter' reaches Period value go to A2
A_Task_Ptr = &A2;
//-------------------
}
//-----------------------------------------------------------------
void A2(void) // SPARE (not used)
//-----------------------------------------------------------------
{
//-------------------
//the next time CpuTimer0 'counter' reaches Period value go to A3
A_Task_Ptr = &A1;
//-------------------
}
//-----------------------------------------
void A3(void) // SPARE (not used)
//-----------------------------------------
{
//-----------------
//the next time CpuTimer0 'counter' reaches Period value go to A1
A_Task_Ptr = &A1;
//-----------------
}
//=================================================================================
// B - TASKS (executed in every 5 msec)
//=================================================================================
//----------------------------------- USER ----------------------------------------
//----------------------------------------
void B1(void) // Toggle GPIO-34
//----------------------------------------
{
if(RunBLDC_Int==1)
{
if(LedBlinkCnt==0)
{
GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1; //turn on/off LD3 on the controlCARD
LedBlinkCnt=50;
}
else
LedBlinkCnt--;
}
else
{
if(LedBlinkCnt==0)
{
GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1; //turn on/off LD3 on the controlCARD
LedBlinkCnt=100;
}
else
LedBlinkCnt--;
}
Gui.VdcBus = ( (long) AdcResult.ADCRESULT6 * (long) K_VdcBus ) >> 12;
if(Gui.VdcBus < Gui.Min_VDC)
{
Gui.OverVoltage = 0;
}
else if(Gui.VdcBus > Gui.Max_VDC)
{
Gui.OverVoltage = 2;
}
else
{
Gui.OverVoltage = 1;
}
if(Gui.OverVoltage != 1)
{
EPwm1Regs.TZFRC.bit.OST = 1;
EPwm2Regs.TZFRC.bit.OST = 1;
EPwm3Regs.TZFRC.bit.OST = 1;
}
//ignore FAULTn when disabled
//There is a blip on this pin when the DRV8301 ENABLE is de-asserted
if((GpioDataRegs.GPADAT.bit.GPIO14 == 0) && RunBLDC_Int)
{
Gui.DRVFaultFlag=1;
}
if(GpioDataRegs.GPADAT.bit.GPIO13 == 1)
{
Gui.DRVOTWFlag = 0;
}
else
{
Gui.DRVOTWFlag = 1;
}
//-----------------
//the next time CpuTimer1 'counter' reaches Period value go to B2
B_Task_Ptr = &B2;
//-----------------
}
//----------------------------------------
void B2(void) // SPARE
//----------------------------------------
{
//-----------------
//the next time CpuTimer1 'counter' reaches Period value go to B3
B_Task_Ptr = &B1;
//-----------------
}
//----------------------------------------
void B3(void) // SPARE
//----------------------------------------
{
//-----------------
//the next time CpuTimer1 'counter' reaches Period value go to B1
B_Task_Ptr = &B1;
//-----------------
}
//MainISR
interrupt void MainISR(void)
{
_iq IDCfdbk;
_iq iqVaIn;
_iq iqVbIn;
_iq iqVcIn;
_iq iqIA;
float ADCValue; //ADC Signal value from throttle
float normSpeed; //convert speed between 0 and .89
GpioDataRegs.GPASET.bit.GPIO22 = 1;
// Verifying the ISR
IsrTicker++;
if(RunBLDC_Int==0)
{
Gui_DBUFF_init();
}
// PMSM Motor
if (RunBLDC_Int==1 && Gui.VdcBus>Gui.Min_VDC && Gui.VdcBus<Gui.Max_VDC)
{
if(CALIBRATE_FLAG)
{
// ------------------------------------------------------------------------------
// ADC conversion and offset adjustment
// ------------------------------------------------------------------------------
iqVaIn = _IQ15toIQ((AdcResult.ADCRESULT1<<3))-InstaSPIN_BLDC1.VaOffset;
iqVbIn = _IQ15toIQ((AdcResult.ADCRESULT2<<3))-InstaSPIN_BLDC1.VbOffset;
iqVcIn = _IQ15toIQ((AdcResult.ADCRESULT3<<3))-InstaSPIN_BLDC1.VcOffset;
iqIA=(_IQ15toIQ(AdcResult.ADCRESULT4<<3)-IA_offset)<<1;
IDCfdbk=(_IQ15toIQ(AdcResult.ADCRESULT5<<3)-IDC_offset)<<1;
// ------------------------------------------------------------------------------
// LPF to average the calibration offsets
// Use the offsets calculated here to initialize BemfA_offset, BemfB_offset
// and BemfC_offset so that they are used for the remaining build levels
// ------------------------------------------------------------------------------
InstaSPIN_BLDC1.VaOffset = _IQmpy(cal_filt_gain,iqVaIn) + InstaSPIN_BLDC1.VaOffset;
InstaSPIN_BLDC1.VbOffset = _IQmpy(cal_filt_gain,iqVbIn) + InstaSPIN_BLDC1.VbOffset;
InstaSPIN_BLDC1.VcOffset = _IQmpy(cal_filt_gain,iqVcIn) + InstaSPIN_BLDC1.VcOffset;
IA_offset = _IQmpy(cal_filt_gain,iqIA) + IA_offset;
IDC_offset = _IQmpy(cal_filt_gain,IDCfdbk) + IDC_offset;
// ------------------------------------------------------------------------------
// force all PWMs to 0% duty cycle
// ------------------------------------------------------------------------------
PHASE_A_ON;
PHASE_B_ON;
PHASE_C_ON;
EPwm1Regs.CMPA.half.CMPA=0; // PWM 1A - PhaseA
EPwm2Regs.CMPA.half.CMPA=0; // PWM 2A - PhaseB
EPwm3Regs.CMPA.half.CMPA=0; // PWM 3A - PhaseC
CALIBRATE_FLAG++;
CALIBRATE_FLAG &= CALIBRATE_TIME;
}
else
{
// ------------------------------------------------------------------------------
// ADC conversion and offset adjustment
// ------------------------------------------------------------------------------
iqVaIn = _IQ15toIQ((AdcResult.ADCRESULT1<<3));
iqVbIn = _IQ15toIQ((AdcResult.ADCRESULT2<<3));
iqVcIn = _IQ15toIQ((AdcResult.ADCRESULT3<<3));
iqIA=(_IQ15toIQ(AdcResult.ADCRESULT4<<3)-IA_offset)<<1;
#if defined (DRV8312)
IDCfdbk=(_IQ15toIQ(AdcResult.ADCRESULT5<<3)-IDC_offset)<<1;
#endif
#if defined(DRV8301) || defined(DRV8302)
IDCfdbk=-((_IQ15toIQ(AdcResult.ADCRESULT5<<3)-IDC_offset)<<1);
#endif
// ------------------------------------------------------------------------------
// Connect inputs of the MOD6 module and call the Modulo 6 counter macro.
// ------------------------------------------------------------------------------
if(Gui.Ref > _IQ(0.0))
{
mod_dir1.CntDirection = _IQ(1.0);
}
else
{
mod_dir1.CntDirection = _IQ(-1.0);
}
PreviousState = mod_dir1.Counter;
MOD6CNTDIR_MACRO(mod_dir1)
// ------------------------------------------------------------------------------
// Connect inputs of the SPEED_PR module and call the speed calculation macro.
// ------------------------------------------------------------------------------
//while counting up we want positive speed
if((mod_dir1.Counter==5)&&(PreviousState==4)&&(mod_dir1.TrigInput))
{
speed1.TimeStamp = VirtualTimer;
SPEED_PR_MACRO(speed1);
SpeedLoopFlag = TRUE;
}
//while counting down we want negative speed
else if((mod_dir1.Counter==0)&&(PreviousState==1)&&(mod_dir1.TrigInput))
{
speed1.TimeStamp = VirtualTimer;
SPEED_PR_MACRO(speed1);
speed1.Speed = _IQmpy(speed1.Speed,_IQ(-1.0));
speed1.SpeedRpm = _IQmpy(speed1.SpeedRpm,_IQ(-1.0));
SpeedLoopFlag = TRUE;
}
// ------------------------------------------------------------------------------
// Connect inputs of the INSTASPIN_BLDC module and call the INSTASPIN_BLDC function.
// ------------------------------------------------------------------------------
InstaSPIN_BLDC1.Vag = iqVaIn - InstaSPIN_BLDC1.VaOffset; // Adjust for offset of Va_in
InstaSPIN_BLDC1.Vbg = iqVbIn - InstaSPIN_BLDC1.VbOffset; // Adjust for offset of Vb_in
InstaSPIN_BLDC1.Vcg = iqVcIn - InstaSPIN_BLDC1.VcOffset; // Adjust for offset of Vc_in
InstaSPIN_BLDC1.State = mod_dir1.Counter; // Update the state
InstaSPIN_BLDC(&InstaSPIN_BLDC1);
mod_dir1.TrigInput = InstaSPIN_BLDC1.Comm_Trig;
if((ClosedCommutationFlag == 0) || (SpeedLoopFlag == FALSE))
{
// ------------------------------------------------------------------------------
// Connect inputs of the RMP3 module and call the Ramp control 3 macro.
// ------------------------------------------------------------------------------
// rmp3.DesiredInput = CmtnPeriodTarget;
RC3_MACRO(rmp3)
// ------------------------------------------------------------------------------
// Connect inputs of the IMPULSE module and call the Impulse macro.
// ------------------------------------------------------------------------------
impl1.Period = rmp3.Out;
IMPULSE_MACRO(impl1)
// ------------------------------------------------------------------------------
// Connect inputs of the MOD6 module and call the Modulo 6 counter macro.
// ------------------------------------------------------------------------------
mod_dir1.TrigInput = impl1.Out;
//using advanced startup to count commutation matches?
if(Gui.AdvancedStartup)
{
//When the BEMF signals it's time to commutate, compare
//against the forced commutation period
if(InstaSPIN_BLDC1.Comm_Trig)
{
BemfLastTrigCnt = BemfTrigCnt;
BemfTrigCnt = 0;
//check if the forced commutation period and the BEMF commutation period
//are within the allowed error window
if(labs(BemfLastTrigCnt - impl1.Period) < GoodTrigCntTrip)
{
GoodTrigCnt++;
}
else
{
GoodTrigCnt = 0;
}
BemfLastTrigCnt = 0;
}
else
{
BemfTrigCnt++;
}
//Check if there are enough commutation matches to switch to closed commutation mode
if(GoodTrigCnt > Gui.TripCnt)
{
ClosedCommutationFlag = 1;
}
}
//if we're not using advanced startup just switch to closed
//commutation mode at the end of the startup ramp.
else if(rmp3.Ramp3DoneFlag != 0)
{
ClosedCommutationFlag = 1;
}
}
switch(control_mode)
{
case VOLTAGE:
if(ClosedCommutationFlag == 0)
{
SpeedLoopFlag = 1; //no need to wait for speed feedback update in this mode.
rc1.SetpointValue = _IQmpy(Gui.DfuncStartup,mod_dir1.CntDirection);
}
else
{
// ------------------------------------------------------------------------------
// Connect inputs of the RMP module and call the Ramp control macro.
// ------------------------------------------------------------------------------
rc1.TargetValue = Gui.Ref;
RC_MACRO(rc1)
}
// ------------------------------------------------------------------------------
// Connect inputs of the PWM_DRV module and call the PWM signal generation
// update macro.
// ------------------------------------------------------------------------------
pwmcntl1.State = (int16)mod_dir1.Counter;
pwmcntl1.Duty = rc1.SetpointValue;
PWM_CNTL_MACRO(pwmcntl1)
break;
case CURRENT:
IRef = Gui.Ref;
if(ClosedCommutationFlag == 0)
{
SpeedLoopFlag = 1; //no need to wait for speed feedback update in this mode.
IRef = _IQmpy(Gui.CurrentStartup,mod_dir1.CntDirection); //use startup current during initial ramp
}
// ------------------------------------------------------------------------------
// Connect inputs of the PID_REG3 module and call the PID current controller
// macro.
// ------------------------------------------------------------------------------
pid1_idc.term.Ref = IRef;
pid1_idc.term.Fbk = _IQmpy(IDCfdbk,mod_dir1.CntDirection);
PID_GR_MACRO(pid1_idc)
// ------------------------------------------------------------------------------
// Connect inputs of the PWM_DRV module and call the PWM signal generation
// update macro.
// ------------------------------------------------------------------------------
pwmcntl1.State = (int16)mod_dir1.Counter;
pwmcntl1.Duty = pid1_idc.term.Out;
PWM_CNTL_MACRO(pwmcntl1)
break;
case VELOCITY:
SpeedRef = Gui.Ref;
// ------------------------------------------------------------------------------
// Connect inputs of the PID_REG3 module and call the PID current controller
// macro.
// ------------------------------------------------------------------------------
pwmcntl1.State = (int16)mod_dir1.Counter;
// Switch from fixed duty-cycle or controlled Speed duty-cycle by SpeedLoopFlag variable
if((ClosedCommutationFlag == 0) || (SpeedLoopFlag == FALSE))
{
pwmcntl1.Duty = _IQmpy(Gui.DfuncStartup,mod_dir1.CntDirection); // fixed duty-cycle
}
else
{
// ------------------------------------------------------------------------------
// Connect inputs of the PID_REG3 module and call the PID speed controller
// macro.
// ------------------------------------------------------------------------------
pid1_spd.term.Ref = SpeedRef;
pid1_spd.term.Fbk = speed1.Speed;
PID_GR_MACRO(pid1_spd)
pwmcntl1.Duty = pid1_spd.term.Out; // controlled Speed duty-cycle
}
PWM_CNTL_MACRO(pwmcntl1)
break;
case CASCADE:
SpeedRef = Gui.Ref;
// ------------------------------------------------------------------------------
// Connect inputs of the PID_REG3 module and call the PID current controller
// macro.
// ------------------------------------------------------------------------------
if((ClosedCommutationFlag == 0) || (SpeedLoopFlag == FALSE))
{
pid1_idc.term.Ref = _IQmpy(Gui.CurrentStartup,mod_dir1.CntDirection);
}
else
{
// ------------------------------------------------------------------------------
// Connect inputs of the PID_REG3 module and call the PID speed controller
// macro.
// ------------------------------------------------------------------------------
pid1_spd.term.Ref = SpeedRef;
pid1_spd.term.Fbk = speed1.Speed;
PID_GR_MACRO(pid1_spd)
pid1_idc.term.Ref = pid1_spd.term.Out;
}
pid1_idc.term.Fbk = _IQmpy(IDCfdbk,mod_dir1.CntDirection);
PID_GR_MACRO(pid1_idc)
// ------------------------------------------------------------------------------
// Connect inputs of the PWM_DRV module and call the PWM signal generation
// update macro.
// ------------------------------------------------------------------------------
pwmcntl1.State = (int16)mod_dir1.Counter;
pwmcntl1.Duty = pid1_idc.term.Out;
PWM_CNTL_MACRO(pwmcntl1)
break;
default:
// ------------------------------------------------------------------------------
// Connect inputs of the PWM_DRV module and call the PWM signal generation
// update macro.
// ------------------------------------------------------------------------------
pwmcntl1.State = 0;
pwmcntl1.Duty = 0;
PWM_CNTL_MACRO(pwmcntl1)
break;
}
//Filter the displayed speed
Gui.Speed = _IQmpy(spd_filt_gain,speed1.Speed - Gui.Speed) + Gui.Speed;
Gui.SpeedRPM = _IQmpy(speed1.BaseRpm,Gui.Speed);
// ------------------------------------------------------------------------------
// Connect inputs of the PWMDAC module
// ------------------------------------------------------------------------------
/* PwmDacCh1 = _IQtoQ15(InstaSPIN_BLDC1.V_int);
PwmDacCh2 = _IQtoQ15(InstaSPIN_BLDC1.Vag);
PwmDacCh3 = _IQtoQ15(iqIA);
#if defined(DRV8301) || defined(DRV8302)
PwmDacCh4 = _IQtoQ15(InstaSPIN_BLDC1.V_int);
#endif*/
PwmDacCh1 = _IQtoQ15(InstaSPIN_BLDC1.V_int);
PwmDacCh2 = (int16)(mod_dir1.Counter * 4096.0L);
PwmDacCh3 = (int16)(GoodTrigCnt * 4096.0L);
#if defined(DRV8301) || defined(DRV8302)
PwmDacCh4 = (int16)impl1.Out;
#endif
// ------------------------------------------------------------------------------
// Connect inputs of the DATALOG module
// ------------------------------------------------------------------------------
DlogCh1 = InstaSPIN_BLDC1.V_int;
DlogCh2 = InstaSPIN_BLDC1.Vag;
DlogCh3 = iqIA;
// ------------------------------------------------------------------------------
// Increase virtual timer and force 15 bit wrap around
// ------------------------------------------------------------------------------
VirtualTimer++;
VirtualTimer &= 0x00007FFF;
// Gui.SpeedRPM = speed1.SpeedRpm;
Gui.CurrentDisplay = IDCfdbk;
InstaSPIN_BLDC1.Int_Threshold = Gui.Threshold;
}
}
// ------------------------------------------------------------------------------
// Call the PWMDAC update macro.
// ------------------------------------------------------------------------------
PWMDAC_MACRO(pwmdac1)
// ------------------------------------------------------------------------------
// Call the DATALOG update function.
// ------------------------------------------------------------------------------
Graph_Data_Update(&gdata);
GpioDataRegs.GPACLEAR.bit.GPIO22 = 1;
#if (DSP2803x_DEVICE_H==1)||(DSP280x_DEVICE_H==1)||(F2806x_DEVICE_H==1)
AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; // Clear ADCINT1 flag reinitialize for next SOC
// Acknowledge interrupt to recieve more interrupts from PIE group 1
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
#endif
}
void Gui_DBUFF_init()
{
if(DlogCurrElementIndex!=gdata.size)
{
*dlogptr1=0;
dlogptr1++;
*dlogptr2=0;
dlogptr2++;
*dlogptr3=0;
dlogptr3++;
DlogCurrElementIndex++;
}
else
{
dlogptr1=DLOG_4CH_buff1;
dlogptr2=DLOG_4CH_buff2;
dlogptr3=DLOG_4CH_buff3;
DlogCurrElementIndex=0;
}
}
//===========================================================================
// No more.
//===========================================================================