Hi,
I have been using C2000 delfino boards and trying to implement a previously developed C library on it.
The problem is that the library uses uint8_t datatype , also arrays and pointer arithmetics on this datatype. I have seen that there is a __byte intrinsic which can be used to access uint8_t datatype. But, how do I implement all the pointer operations like dereferencing etc. using this function?
Regards,
Apoorv