This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377D: adc_soc_continuous in 28377D

Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE

Tool/software: Code Composer Studio

hi everyone.i found a questions about  adc_soc_continuous in controsuite,i adjust the channel to A2,when i run the codes,the codes stop at "while(0 == AdcaRegs.ADCINTFLG.bit.ADCINT3);",i know the ADCINT3 are set at " AdcaRegs.ADCINTSEL3N4.bit.INT3SEL = 7;  //end of SOC7 will set INT3 flag".so i can not understand why the codes run in dead loop.i change nothing but only the channel.does somebodykonw the reason?thank you very much.

follow by the code.

//###########################################################################
//
// FILE:   adc_soc_continuous_cpu01.c
//
// TITLE:  ADC continuous self-triggering for F2837xD.
//
//! \addtogroup cpu01_example_list
//! <h1> ADC Continuous Triggering (adc_soc_continuous)</h1>
//!
//! This example sets up the ADC to convert continuously, achieving maximum
//! sampling rate.\n
//!
//! After the program runs, the memory will contain:
//!
//! - \b AdcaResults \b: A sequence of analog-to-digital conversion samples
//! from pin A0. The time between samples is the minimum possible based on the
//! ADC speed.
//
//###########################################################################
// $TI Release: F2837xD Support Library v210 $
// $Release Date: Tue Nov  1 14:46:15 CDT 2016 $
// $Copyright: Copyright (C) 2013-2016 Texas Instruments Incorporated -
//             http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################
//
// Included Files
//
#include "F28x_Project.h"
//
// Function Prototypes
//
void ConfigureADC(void);
void SetupADCContinuous(Uint16 channel);
//
// Defines
//
#define RESULTS_BUFFER_SIZE 256 //buffer for storing conversion results
                                //(size must be multiple of 16)
//
// Globals
//
Uint16 AdcaResults[RESULTS_BUFFER_SIZE];
Uint16 resultsIndex;
void main(void)
{
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xD_SysCtrl.c file.
//
    InitSysCtrl();
//
// Step 2. Initialize GPIO:
// This example function is found in the F2837xD_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
    InitGpio(); // Skipped for this example
//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
    DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xD_PieCtrl.c file.
//
    InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
    IER = 0x0000;
    IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_DefaultIsr.c.
// This function is found in F2837xD_PieVect.c.
//
    InitPieVectTable();
//
// Configure the ADC and power it up
//
    ConfigureADC();
//
// Setup the ADC for continuous conversions on channel 0
//
    SetupADCContinuous(2);
//
// Enable global Interrupts and higher priority real-time debug events:
//
    EINT;  // Enable Global interrupt INTM
    ERTM;  // Enable Global realtime interrupt DBGM
//
// Initialize results buffer
//
    for(resultsIndex = 0; resultsIndex < RESULTS_BUFFER_SIZE; resultsIndex++)
    {
        AdcaResults[resultsIndex] = 0;
    }
    resultsIndex = 0;
//
// take conversions indefinitely in loop
//
    do
    {
        //
        //enable ADCINT flags
        //
        AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1;
        AdcaRegs.ADCINTSEL1N2.bit.INT2E = 1;
        AdcaRegs.ADCINTSEL3N4.bit.INT3E = 1;
        AdcaRegs.ADCINTSEL3N4.bit.INT4E = 1;
        AdcaRegs.ADCINTFLGCLR.all = 0x000F;
        //
        //initialize results index
        //
        resultsIndex = 0;
        //
        //software force start SOC0 to SOC7
        //
        AdcaRegs.ADCSOCFRC1.all = 0x00FF;
        //
        //keep taking samples until the results buffer is full
        //
        while(resultsIndex < RESULTS_BUFFER_SIZE)
        {
            //
            //wait for first set of 8 conversions to complete
            //
            while(0 == AdcaRegs.ADCINTFLG.bit.ADCINT3);
            //
            //clear both INT flags generated by first 8 conversions
            //
            AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
            AdcaRegs.ADCINTFLGCLR.bit.ADCINT3 = 1;
            //
            //save results for first 8 conversions
            //
            //note that during this time, the second 8 conversions have
            //already been triggered by EOC6->ADCIN1 and will be actively
            //converting while first 8 results are being saved
            //
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT0;
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT1;
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT2;
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT3;
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT4;
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT5;
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT6;
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT7;
            //
            //wait for the second set of 8 conversions to complete
            //
            while(0 == AdcaRegs.ADCINTFLG.bit.ADCINT4);
            //
            //clear both INT flags generated by second 8 conversions
            //
            AdcaRegs.ADCINTFLGCLR.bit.ADCINT2 = 1;
            AdcaRegs.ADCINTFLGCLR.bit.ADCINT4 = 1;
            //
            //save results for second 8 conversions
            //
            //note that during this time, the first 8 conversions have
            //already been triggered by EOC14->ADCIN2 and will be actively
            //converting while second 8 results are being saved
            //
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT8;
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT9;
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT10;
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT11;
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT12;
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT13;
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT14;
            AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT15;
        }
        //
        //disable all ADCINT flags to stop sampling
        //
        AdcaRegs.ADCINTSEL1N2.bit.INT1E = 0;
        AdcaRegs.ADCINTSEL1N2.bit.INT2E = 0;
        AdcaRegs.ADCINTSEL3N4.bit.INT3E = 0;
        AdcaRegs.ADCINTSEL3N4.bit.INT4E = 0;
        //
        //at this point, AdcaResults[] contains a sequence of conversions
        //from the selected channel
        //
        //
        //software breakpoint, hit run again to get updated conversions
        //
        asm("   ESTOP0");
    }while(1);
}
//
// ConfigureADC - Write ADC configurations and power up the ADC for both
//                ADC A and ADC B
//
void ConfigureADC(void)
{
    EALLOW;
    //
    //write configurations
    //
    AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4
    AdcSetMode(ADC_ADCA, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);
    //
    //Set pulse positions to late
    //
    AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;
    //
    //power up the ADC
    //
    AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;
    //
    //delay for 1ms to allow ADC time to power up
    //
    DELAY_US(1000);
    EDIS;
}
//
// SetupADCContinuous - setup the ADC to continuously convert on one channel
//
void SetupADCContinuous(Uint16 channel)
{
    Uint16 acqps;
    //
    //determine minimum acquisition window (in SYSCLKS) based on resolution
    //
    if(ADC_RESOLUTION_12BIT == AdcaRegs.ADCCTL2.bit.RESOLUTION)
    {
        acqps = 14; //75ns
    }
    else //resolution is 16-bit
    {
        acqps = 63; //320ns
    }
    EALLOW;
    AdcaRegs.ADCSOC0CTL.bit.CHSEL  = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC1CTL.bit.CHSEL  = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC2CTL.bit.CHSEL  = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC3CTL.bit.CHSEL  = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC4CTL.bit.CHSEL  = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC5CTL.bit.CHSEL  = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC6CTL.bit.CHSEL  = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC7CTL.bit.CHSEL  = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC8CTL.bit.CHSEL  = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC9CTL.bit.CHSEL  = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC10CTL.bit.CHSEL = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC11CTL.bit.CHSEL = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC12CTL.bit.CHSEL = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC13CTL.bit.CHSEL = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC14CTL.bit.CHSEL = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC15CTL.bit.CHSEL = channel;  //SOC will convert on channel
    AdcaRegs.ADCSOC0CTL.bit.ACQPS  = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCSOC1CTL.bit.ACQPS  = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCSOC2CTL.bit.ACQPS  = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCSOC3CTL.bit.ACQPS  = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCSOC4CTL.bit.ACQPS  = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCSOC5CTL.bit.ACQPS  = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCSOC6CTL.bit.ACQPS  = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCSOC7CTL.bit.ACQPS  = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCSOC9CTL.bit.ACQPS  = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCSOC10CTL.bit.ACQPS = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCSOC11CTL.bit.ACQPS = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCSOC12CTL.bit.ACQPS = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCSOC13CTL.bit.ACQPS = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCSOC14CTL.bit.ACQPS = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCSOC15CTL.bit.ACQPS = acqps;    //sample window is acqps +
                                               //1 SYSCLK cycles
    AdcaRegs.ADCINTSEL1N2.bit.INT1E = 0; //disable INT1 flag
    AdcaRegs.ADCINTSEL1N2.bit.INT2E = 0; //disable INT2 flag
    AdcaRegs.ADCINTSEL3N4.bit.INT3E = 0; //disable INT3 flag
    AdcaRegs.ADCINTSEL3N4.bit.INT4E = 0; //disable INT4 flag
    AdcaRegs.ADCINTSEL1N2.bit.INT1CONT = 0;
    AdcaRegs.ADCINTSEL1N2.bit.INT2CONT = 0;
    AdcaRegs.ADCINTSEL3N4.bit.INT3CONT = 0;
    AdcaRegs.ADCINTSEL3N4.bit.INT4CONT = 0;
    AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 6;  //end of SOC6 will set INT1 flag
    AdcaRegs.ADCINTSEL1N2.bit.INT2SEL = 14; //end of SOC14 will set INT2 flag
    AdcaRegs.ADCINTSEL3N4.bit.INT3SEL = 7;  //end of SOC7 will set INT3 flag
    AdcaRegs.ADCINTSEL3N4.bit.INT4SEL = 15; //end of SOC15 will set INT4 flag
    //
    //ADCINT2 will trigger first 8 SOCs
    //
    AdcaRegs.ADCINTSOCSEL1.bit.SOC0 = 2;
    AdcaRegs.ADCINTSOCSEL1.bit.SOC1 = 2;
    AdcaRegs.ADCINTSOCSEL1.bit.SOC2 = 2;
    AdcaRegs.ADCINTSOCSEL1.bit.SOC3 = 2;
    AdcaRegs.ADCINTSOCSEL1.bit.SOC4 = 2;
    AdcaRegs.ADCINTSOCSEL1.bit.SOC5 = 2;
    AdcaRegs.ADCINTSOCSEL1.bit.SOC6 = 2;
    AdcaRegs.ADCINTSOCSEL1.bit.SOC7 = 2;
    //
    //ADCINT1 will trigger second 8 SOCs
    //
    AdcaRegs.ADCINTSOCSEL2.bit.SOC8 = 1;
    AdcaRegs.ADCINTSOCSEL2.bit.SOC9 = 1;
    AdcaRegs.ADCINTSOCSEL2.bit.SOC10 = 1;
    AdcaRegs.ADCINTSOCSEL2.bit.SOC11 = 1;
    AdcaRegs.ADCINTSOCSEL2.bit.SOC12 = 1;
    AdcaRegs.ADCINTSOCSEL2.bit.SOC13 = 1;
    AdcaRegs.ADCINTSOCSEL2.bit.SOC14 = 1;
    AdcaRegs.ADCINTSOCSEL2.bit.SOC15 = 1;
    EDIS;
}
//
// End of file
//