Other Parts Discussed in Thread: TMS320F28379D, AMC1305M05, CONTROLSUITE
Hi community, I got problems to get the right data out of the Sigma-Delta Filter Module. The bitstream is made by a AMC1305M05 from TI. For filtering I use the integrated SDFM of a TMS320F28379D (ControlCard Version with Docking-Station).
Both sides need a CLK to work correctly and I configured a ePWM-Module on the TMS320F28379D for this. The CLK running with 20 MHz to get detailed data by the most speed.
Now the hardware is adjust to work fine with less as possible noise on the filtered signal.
For the first test I used a project out of the ControlSuite "sdfm_pwm_sync". The basic configuration of every SDFM-Data-Filter is a OSR of 64 and Bitshift of 4 Bits let get me exact values, but all Data is in a signed Integer (correct?) Two´s Complement.
At the use of the original Code in CodeComposerStudio there can I also see, that there is a problem with this Data-Type, because CCS interprets everything as unsigned integer. This wrong interpretation also happen, when the data was saved out of the CCS into a csv-file. (Only binaräy Code was right.)
1.How can I easy convert the data to a correct unsigend integer to use the data fast as possible? For example in a inerrupt to oush the data to a register of dac or something else.
The next is that after ~ 200 samples out of the SDFM a peak in the data happens and it can jump to maximum or to the minimum. At first I thought it was a problem at saving the data, because I decided to save more than to 200 samples (in the orignal code 200 data points was the max). Than I changed the code so that the data is not saved on the board and instead a DAC reproduce out of the digital data the orignal waveform. I thought that this will helps agains the peaks, but the peaks are still there. I estimated that peaks still happens after every 200 Sample.
2. What is wrong in my data processing? How can I stop the peaks?
I will give a example scrrenshot from oscilloscope where you can see three Signals produces by DACs. The DACs are feed with data out out of the SDFM of the TMS320F28379D and the bitstream comes from three AMC1305M05 ICs. The measured signal by AMC1305M05 ICs comes from a single signal generator over a voltage divider.
//###########################################################################
//
// FILE: sdfm_pwm_sync_cpu_cpu01.c
//
// TITLE: SDFM PWM sync Example for F2837xD.
//
//! \addtogroup cpu01_example_list
//! <h1> SDFM PWM Sync </h1>
//!
//! In this example, SDFM filter data is read by CPU in SDFM ISR routine. The
//! SDFM configuration is shown below:
//! - SDFM1 is used in this example
//! - MODE0 Input control mode selected
//! - Comparator settings
//! - Sinc3 filter selected
//! - OSR = 32
//! - HLT = 0x7FFF (Higher threshold setting)
//! - LLT = 0x0000(Lower threshold setting)
//! - Data filter settings
//! - All the 4 filter modules enabled
//! - Sinc3 filter selected
//! - OSR = 256
//! - All the 4 filters are synchronized by using PWM
//! (Master Filter enable bit)
//! - Filter output represented in 16 bit format
//! - In order to convert 25 bit Data filter
//! into 16 bit format user needs to right shift by 9 bits for
//! Sinc3 filter with OSR = 256
//! - Interrupt module settings for SDFM filter
//! - All the 4 higher threshold comparator interrupts disabled
//! - All the 4 lower threshold comparator interrupts disabled
//! - All the 4 modulator failure interrupts disabled
//! - All the 4 filter will generate interrupt when a new filter data
//! is available
//!
//
//###########################################################################
// $TI Release: F2837xD Support Library v210 $
// $Release Date: Tue Nov 1 14:46:15 CDT 2016 $
// $Copyright: Copyright (C) 2013-2016 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################
//
// Included Files
//
#include "F28x_Project.h"
#include "F2837xD_struct.h"
#include "F2837xD_sdfm_drivers.h"
//
// Defines
//
#define MAX_SAMPLES 200
#define SDFM_PIN_MUX_OPTION1 1
#define SDFM_PIN_MUX_OPTION2 2
#define SDFM_PIN_MUX_OPTION3 3
#define EPWM_TIMER_TBPRD 65535 // ePWM Period register
///////////////////////////////////////////////////////////////////////////////
//Define für ePWM
#define DB_UP 1
//Define für DAC
#define REFERENCE_VDAC 0
#define REFERENCE_VREF 1
#define DACA 1
#define DACB 2
#define DACC 3
#define REFERENCE REFERENCE_VREF
#define DAC_NUM DACA
//////////////////////////////////////////////////////////////////////////////
//
// Globals
//
uint16_t gPeripheralNumber, gPWM_number = 11;
uint16_t Filter1_Result[MAX_SAMPLES];
uint16_t Filter3_Result[MAX_SAMPLES];
uint16_t Filter2_Result[MAX_SAMPLES];
uint16_t Filter4_Result[MAX_SAMPLES];
//////////////////////////////////////////////////////
//Globales für ePWM
Uint16 EPwm7_DB_Direction;
Uint16 EPwm6_DB_Direction;
Uint16 EPwm5_DB_Direction;
Uint16 EPwm4_DB_Direction;
Uint32 EPwm7TZIntCount;
Uint32 EPwm6TZIntCount;
Uint32 EPwm5TZIntCount;
Uint32 EPwm4TZIntCount;
//Glaobales für DAC
volatile struct DAC_REGS* DAC_PTR[4] = {0x0,&DacaRegs,&DacbRegs,&DaccRegs};
/////////////////////////////////////////////////////
#pragma DATA_SECTION(Filter1_Result,"Filter1_RegsFile");
#pragma DATA_SECTION(Filter2_Result,"Filter2_RegsFile");
#pragma DATA_SECTION(Filter3_Result,"Filter3_RegsFile");
#pragma DATA_SECTION(Filter4_Result,"Filter4_RegsFile");
//
// Function Prototypes
//
void Sdfm_configurePins(uint16_t);
void InitEPwm(void);
void done(void);
__interrupt void Sdfm1_ISR(void);
__interrupt void Sdfm2_ISR(void);
///////////////////////////////////////////////////////
//Function Prototypes für ePWM
void InitEPwm7Example();
void InitEPwm6Example();
void InitEPwm5Example();
void InitEPwm4Example();
__interrupt void epwm7_isr(void);
__interrupt void epwm6_isr(void);
__interrupt void epwm5_isr(void);
__interrupt void epwm4_isr(void);
void InitEPwmGpio_TZ(void);
//Function Prototypes für DAC
void configureDAC(Uint16 dac_num);
///////////////////////////////////////////////////////
//
// Main
//
void main(void)
{
uint16_t pinMuxoption;
uint16_t HLT, LLT;
//
// Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xD_SysCtrl.c file.
//
InitSysCtrl();
/////////////////////////////////////////////////
InitGpio();
// Einschalten der CLKs der PWM-Module
//
CpuSysRegs.PCLKCR2.bit.EPWM7=1;
CpuSysRegs.PCLKCR2.bit.EPWM6=1;
CpuSysRegs.PCLKCR2.bit.EPWM5=1;
CpuSysRegs.PCLKCR2.bit.EPWM4=1;
InitEPwmGpio_TZ();
/////////////////////////////////////////////////
//
// Clear all __interrupts and initialize PIE vector table:
// Disable CPU __interrupts
//
DINT;
//
// Initialize PIE control registers to their default state.
// The default state is all PIE __interrupts disabled and flags
// are cleared.
// This function is found in the F2837xD_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU __interrupts and clear all CPU __interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the __interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_SysCtrl.c.
// This function is found in F2837xD_SysCtrl.c.
//
InitPieVectTable();
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
EALLOW;
PieVectTable.SD1_INT = &Sdfm1_ISR;
PieVectTable.SD2_INT = &Sdfm2_ISR;
/////////////////////////////////////////////
PieVectTable.EPWM7_TZ_INT = &epwm7_isr;
PieVectTable.EPWM6_TZ_INT = &epwm6_isr;
PieVectTable.EPWM5_TZ_INT = &epwm5_isr;
PieVectTable.EPWM4_TZ_INT = &epwm4_isr;
////////////////////////////////////////////
EDIS;
EALLOW;
/////////////////////////////////////////////////////////
// Alles zwischen den ******* wird synchron ausgeführt durch die Sync Befehle
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =0;
EDIS;
//Intitialisierung/Einstellung der EPWM2 und der EPWM7
InitEPwm7Example();
InitEPwm6Example();
InitEPwm5Example();
InitEPwm4Example();
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =1;
EDIS;
/////////////////////////////////////////////////////////
//
// Enable CPU INT5 which is connected to SDFM INT
//
IER |= M_INT5;
IER |= M_INT6;//Interrupt für ePWM7
IER |= M_INT4;
IER |= M_INT3;
//
// Enable SDFM INTn in the PIE: Group 5 __interrupt 9-10
//
PieCtrlRegs.PIEIER5.bit.INTx9 = 1; // SDFM1 interrupt enabled
//PieCtrlRegs.PIEIER5.bit.INTx10 = 1; // SDFM2 interrupt enabled
PieCtrlRegs.PIEIER2.bit.INTx7 = 1;
PieCtrlRegs.PIEIER2.bit.INTx6 = 1;
PieCtrlRegs.PIEIER2.bit.INTx5 = 1;
PieCtrlRegs.PIEIER2.bit.INTx4 = 1;
EINT;
#ifdef CPU1
pinMuxoption = SDFM_PIN_MUX_OPTION1;
//
// Configure GPIO pins as SDFM pins
//
Sdfm_configurePins(pinMuxoption);
#endif
//
// Select SDFM1
//
gPeripheralNumber = SDFM1;
//
// Input Control Module
//
// Configure Input Control Mode: Modulator Clock rate = Modulator data rate
//
Sdfm_configureInputCtrl(gPeripheralNumber, FILTER1, MODE_0);
Sdfm_configureInputCtrl(gPeripheralNumber, FILTER2, MODE_0);
Sdfm_configureInputCtrl(gPeripheralNumber, FILTER3, MODE_0);
Sdfm_configureInputCtrl(gPeripheralNumber, FILTER4, MODE_0);
//
// Comparator Module
//
HLT = 0x7FFF; //Over value threshold settings
LLT = 0x0000; //Under value threshold settings
//
// Configure Comparator module's comparator filter type and comparator's OSR
// value, higher threshold, lower threshold
//
Sdfm_configureComparator(gPeripheralNumber, FILTER1, SINC3, OSR_32,
HLT, LLT);
Sdfm_configureComparator(gPeripheralNumber, FILTER2, SINC3, OSR_32,
HLT, LLT);
Sdfm_configureComparator(gPeripheralNumber, FILTER3, SINC3, OSR_32,
HLT, LLT);
Sdfm_configureComparator(gPeripheralNumber, FILTER4, SINC3, OSR_32,
HLT, LLT);
//
// Enable Master filter bit: Unless this bit is set none of the filter modules
// can be enabled. All the filter modules are synchronized when master filter
// bit is enabled after individual filter modules are enabled. All the filter
// modules are asynchronized when master filter bit is enabled before
// individual filter modules are enabled.
//
Sdfm_enableMFE(gPeripheralNumber);
//
// Data filter Module
//
// Configure Data filter modules filter type, OSR value and
// enable / disable data filter
//
Sdfm_configureData_filter(gPeripheralNumber, FILTER1, FILTER_ENABLE, SINC3,
OSR_64, DATA_16_BIT, SHIFT_4_BITS);
Sdfm_configureData_filter(gPeripheralNumber, FILTER2, FILTER_ENABLE, SINC3,
OSR_64, DATA_16_BIT, SHIFT_4_BITS);
Sdfm_configureData_filter(gPeripheralNumber, FILTER3, FILTER_ENABLE, SINC3,
OSR_64, DATA_16_BIT, SHIFT_4_BITS);
Sdfm_configureData_filter(gPeripheralNumber, FILTER4, FILTER_ENABLE, SINC3,
OSR_64, DATA_16_BIT, SHIFT_4_BITS);
//
// PWM11.CMPC, PWM11.CMPD, PWM12.CMPC and PWM12.CMPD signals cannot synchronize
// the filters. This option is not being used in this example.
//
Sdfm_configureExternalreset(gPeripheralNumber,FILTER_1_EXT_RESET_ENABLE,
FILTER_2_EXT_RESET_ENABLE,
FILTER_3_EXT_RESET_ENABLE,
FILTER_4_EXT_RESET_ENABLE);
//
// Init EPWMs
//
InitEPwm();
//
// Enable interrupts
//
// Following SDFM interrupts can be enabled / disabled using this function.
// Enable / disable comparator high threshold
// Enable / disable comparator low threshold
// Enable / disable modulator clock failure
// Enable / disable filter acknowledge
//
Sdfm_configureInterrupt(gPeripheralNumber, FILTER1, IEH_DISABLE,
IEL_DISABLE, MFIE_ENABLE, AE_ENABLE);
Sdfm_configureInterrupt(gPeripheralNumber, FILTER2, IEH_DISABLE,
IEL_DISABLE, MFIE_ENABLE, AE_ENABLE);
Sdfm_configureInterrupt(gPeripheralNumber, FILTER3, IEH_DISABLE,
IEL_DISABLE, MFIE_ENABLE, AE_ENABLE);
Sdfm_configureInterrupt(gPeripheralNumber, FILTER4, IEH_DISABLE,
IEL_DISABLE, MFIE_ENABLE, AE_ENABLE);
while((*EPWM[gPWM_number]).TBCTR < 550);
//
// Enable master interrupt so that any of the filter interrupts can trigger
// by SDFM interrupt to CPU
//
Sdfm_enableMIE(gPeripheralNumber);
////////////////////////////////////////
//Konfiguration von DAC Aufruf
configureDAC(DAC_NUM);
////////////////////////////////////////
while(1);
}
//
// Sdfm1_ISR - SDFM 1 ISR
//
__interrupt void Sdfm1_ISR(void)
{
//uint32_t sdfmReadFlagRegister = 0;
//static uint16_t loopCounter1 = 0;
//
// Read SDFM flag register (SDIFLG)
//
//sdfmReadFlagRegister = Sdfm_readFlagRegister(gPeripheralNumber);
/*
if(loopCounter1 <= MAX_SAMPLES)
{
//
// Read each SDFM filter output and store it in respective filter
// result array
//
Filter1_Result[loopCounter1] = SDFM1_READ_FILTER1_DATA_16BIT;
Filter2_Result[loopCounter1] = SDFM1_READ_FILTER2_DATA_16BIT;
Filter3_Result[loopCounter1] = SDFM1_READ_FILTER3_DATA_16BIT;
Filter4_Result[loopCounter1++] = SDFM1_READ_FILTER4_DATA_16BIT;
//
// Clear SDFM flag register
//
Sdfm_clearFlagRegister(gPeripheralNumber,sdfmReadFlagRegister);
sdfmReadFlagRegister = Sdfm_readFlagRegister(gPeripheralNumber);
if(sdfmReadFlagRegister != 0x0)
{
ESTOP0;
}
}
else
{
ESTOP0;
done();
}
*/
//*******************************************
//Neue Datenverarbeitung mit Ausgabe über DAC
while(1)
{
//Filter1_Result[1] = SDFM2_READ_FILTER1_DATA_16BIT;
DAC_PTR[DACA]->DACVALS.all = SDFM1_READ_FILTER1_DATA_16BIT;
DAC_PTR[DACB]->DACVALS.all = SDFM1_READ_FILTER2_DATA_16BIT;
DAC_PTR[DACC]->DACVALS.all = SDFM1_READ_FILTER3_DATA_16BIT;
//unsigned int val = (unsigned char)SDFM1_READ_FILTER3_DATA_16BIT[0] << 16 | (unsigned char)SDFM1_READ_FILTER3_DATA_16BIT[1];
//DAC_PTR[DACC]->DACVALS.all = val;
}
//*******************************************
//
// Acknowledge this __interrupt to receive more __interrupts from group 5
//
PieCtrlRegs.PIEACK.all = PIEACK_GROUP5;
}
//
// Sdfm2_ISR - SDFM 2 ISR
//
__interrupt void Sdfm2_ISR(void)
{
//uint32_t sdfmReadFlagRegister;
//static uint16_t loopCounter1 = 0;
//
// Read SDFM flag register (SDIFLG)
//
//sdfmReadFlagRegister = Sdfm_readFlagRegister(gPeripheralNumber);
/*
if(loopCounter1 <= MAX_SAMPLES)
{
//
// Read each SDFM filter output and store it in respective filter
// result array
//
Filter1_Result[loopCounter1] = SDFM2_READ_FILTER1_DATA_16BIT;
Filter2_Result[loopCounter1] = SDFM2_READ_FILTER2_DATA_16BIT;
Filter3_Result[loopCounter1] = SDFM2_READ_FILTER3_DATA_16BIT;
Filter4_Result[loopCounter1++] = SDFM2_READ_FILTER4_DATA_16BIT;
//
// Clear SDFM flag register
//
Sdfm_clearFlagRegister(gPeripheralNumber,sdfmReadFlagRegister);
sdfmReadFlagRegister = Sdfm_readFlagRegister(gPeripheralNumber);
if(sdfmReadFlagRegister != 0x0)
{
ESTOP0;
}
}
else
{
ESTOP0;
done();
}
*/
//*******************************************
//Neue Datenverarbeitung mit Ausgabe über DAC
//Filter1_Result[1] = SDFM2_READ_FILTER1_DATA_16BIT;
DAC_PTR[DACA]->DACVALS.all = SDFM1_READ_FILTER1_DATA_16BIT;
DAC_PTR[DACB]->DACVALS.all = SDFM1_READ_FILTER2_DATA_16BIT;
DAC_PTR[DACC]->DACVALS.all = SDFM1_READ_FILTER3_DATA_16BIT;
//*******************************************
//
//
// Acknowledge this __interrupt to receive more __interrupts from group 5
//
PieCtrlRegs.PIEACK.all = PIEACK_GROUP5;
}
//
// Sdfm_configurePins - Configure SDFM GPIOs
//
void Sdfm_configurePins(uint16_t sdfmPinOption)
{
uint16_t pin;
switch (sdfmPinOption)
{
case SDFM_PIN_MUX_OPTION1:
for(pin=16;pin<=31;pin++)
{
GPIO_SetupPinOptions(pin, GPIO_INPUT, GPIO_ASYNC);
GPIO_SetupPinMux(pin,GPIO_MUX_CPU1,7);
}
break;
case SDFM_PIN_MUX_OPTION2:
for(pin=48;pin<=63;pin++)
{
GPIO_SetupPinOptions(pin, GPIO_INPUT, GPIO_ASYNC);
GPIO_SetupPinMux(pin,GPIO_MUX_CPU1,7);
}
break;
case SDFM_PIN_MUX_OPTION3:
for(pin=122;pin<=137;pin++)
{
GPIO_SetupPinOptions(pin, GPIO_INPUT, GPIO_ASYNC);
GPIO_SetupPinMux(pin,GPIO_MUX_CPU1,7);
}
break;
}
}
//
// InitEPwm - Initialize specified EPWM settings
//
void InitEPwm(void)
{
uint16_t CMPC,CMPD;
CMPC = 2;
CMPD = 2;
#ifdef CPU1
GPIO_SetupPinOptions(4, GPIO_OUTPUT, GPIO_ASYNC);
GPIO_SetupPinMux(4,GPIO_MUX_CPU1,1);
#endif
EALLOW;
//
// Allows all users to globally synchronize all enabled ePWM modules to
// the time-base clock (TBCLK)
//
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;
//
// Setup TBCLK
//
(*EPWM[gPWM_number]).TBPHS.bit.TBPHS = 0x0000; // Phase is 0
(*EPWM[gPWM_number]).TBCTR = 0x0000; // Clear counter
(*EPWM[gPWM_number]).TBPRD = EPWM_TIMER_TBPRD; // Set timer period
// 801 TBCLKs.
(*EPWM[gPWM_number]).CMPC = CMPC; // Set Compare C value
(*EPWM[gPWM_number]).CMPD = CMPD; // Set Compare D value
(*EPWM[gPWM_number]).CMPA.bit.CMPA = CMPC; // Set Compare C value
(*EPWM[gPWM_number]).CMPB.bit.CMPB = CMPD; // Set Compare D value
//
// Setup counter mode
//
(*EPWM[gPWM_number]).TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count up
(*EPWM[gPWM_number]).TBCTL.bit.HSPCLKDIV = TB_DIV1;
(*EPWM[gPWM_number]).TBCTL.bit.CLKDIV = TB_DIV1;
//
// Set actions
//
(*EPWM[gPWM_number]).AQCTLA.bit.CAU = 3; // Set PWM1A on event A, up
// count
//
// Set actions
//
(*EPWM[gPWM_number]).AQCTLB.bit.CBU = 3; // Set PWM1A on event A, up
// count
EDIS;
}
//
// done - Function to halt debugger and stop application
//
void done(void)
{
asm(" ESTOP0");
for (;;);
}
//////////////////////////////////////////////////////////////////////////////////////////
void InitEPwmGpio_TZ(void)
{
EALLOW;
GpioCtrlRegs.GPAPUD.bit.GPIO12 = 1; // Disable pull-up on GPIO10 (EPWM7A)
GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 1; // Configure GPIO10 as EPWM7A
GpioCtrlRegs.GPAPUD.bit.GPIO13 = 1; // Disable pull-up on GPIO11 (EPWM7B)
GpioCtrlRegs.GPAMUX1.bit.GPIO13 = 1; // Configure GPIO11 as EPWM7B
GpioCtrlRegs.GPAPUD.bit.GPIO10 = 1; //EPWM6A
GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 1; //
GpioCtrlRegs.GPAPUD.bit.GPIO11 = 1; //EPWM6B
GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 1; //
GpioCtrlRegs.GPAPUD.bit.GPIO8 = 1; //EPWM5A
GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 1; //
GpioCtrlRegs.GPAPUD.bit.GPIO9 = 1; //EPWM5B
GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 1; //
GpioCtrlRegs.GPAPUD.bit.GPIO6 = 1; //EPWM4A
GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 1; //
GpioCtrlRegs.GPAPUD.bit.GPIO7 = 1; //EPWM4B
GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 1; //
EDIS;
}
//
// End of file
//
//EPM7 nur für Test-Zwecke
void InitEPwm7Example()
{
EALLOW;
EPwm7Regs.TBPRD = 4;
EPwm7Regs.TBPHS.bit.TBPHS = 0x0000;
EPwm7Regs.TBCTR = 0x0000;
EPwm7Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
EPwm7Regs.TBCTL.bit.PHSEN = TB_DISABLE;
EPwm7Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm7Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm7Regs.CMPA.bit.CMPA = 2;
EPwm7Regs.AQCTLA.bit.ZRO =AQ_SET;
EPwm7Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EPwm7Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm7Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm7Regs.DBCTL.bit.IN_MODE = DBA_ALL;
EPwm7Regs.DBRED.bit.DBRED = 0;
EPwm7Regs.DBFED.bit.DBFED = 0;
EPwm7_DB_Direction = DB_UP;
EPwm7Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;
EPwm7Regs.ETSEL.bit.INTEN = 1;
EPwm7Regs.ETPS.bit.INTPRD = ET_3RD;
EDIS;
}
__interrupt void epwm7_isr(void)
{
EPwm7Regs.ETCLR.bit.INT = 1;
}
//
//EPM7 nur für Test-Zwecke
void InitEPwm6Example()
{
EALLOW;
EPwm6Regs.TBPRD = 4;
EPwm6Regs.TBPHS.bit.TBPHS = 0x0000;
EPwm6Regs.TBCTR = 0x0000;
EPwm6Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
EPwm6Regs.TBCTL.bit.PHSEN = TB_DISABLE;
EPwm6Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm6Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm6Regs.CMPA.bit.CMPA = 2;
EPwm6Regs.AQCTLA.bit.ZRO =AQ_SET;
EPwm6Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EPwm6Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm6Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm6Regs.DBCTL.bit.IN_MODE = DBA_ALL;
EPwm6Regs.DBRED.bit.DBRED = 0;
EPwm6Regs.DBFED.bit.DBFED = 0;
EPwm6_DB_Direction = DB_UP;
EPwm6Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;
EPwm6Regs.ETSEL.bit.INTEN = 1;
EPwm6Regs.ETPS.bit.INTPRD = ET_3RD;
EDIS;
}
__interrupt void epwm6_isr(void)
{
EPwm6Regs.ETCLR.bit.INT = 1;
}
//
//EPM7 nur für Test-Zwecke
void InitEPwm5Example()
{
EALLOW;
EPwm5Regs.TBPRD = 4;
EPwm5Regs.TBPHS.bit.TBPHS = 0x0000;
EPwm5Regs.TBCTR = 0x0000;
EPwm5Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
EPwm5Regs.TBCTL.bit.PHSEN = TB_DISABLE;
EPwm5Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm5Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm5Regs.CMPA.bit.CMPA = 2;
EPwm5Regs.AQCTLA.bit.ZRO =AQ_SET;
EPwm5Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EPwm5Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm5Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm5Regs.DBCTL.bit.IN_MODE = DBA_ALL;
EPwm5Regs.DBRED.bit.DBRED = 0;
EPwm5Regs.DBFED.bit.DBFED = 0;
EPwm5_DB_Direction = DB_UP;
EPwm5Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;
EPwm5Regs.ETSEL.bit.INTEN = 1;
EPwm5Regs.ETPS.bit.INTPRD = ET_3RD;
EDIS;
}
__interrupt void epwm5_isr(void)
{
EPwm5Regs.ETCLR.bit.INT = 1;
}
//
//EPM7 nur für Test-Zwecke
void InitEPwm4Example()
{
EALLOW;
EPwm4Regs.TBPRD = 4;
EPwm4Regs.TBPHS.bit.TBPHS = 0x0000;
EPwm4Regs.TBCTR = 0x0000;
EPwm4Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
EPwm4Regs.TBCTL.bit.PHSEN = TB_DISABLE;
EPwm4Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm4Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm4Regs.CMPA.bit.CMPA = 2;
EPwm4Regs.AQCTLA.bit.ZRO =AQ_SET;
EPwm4Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EPwm4Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm4Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm4Regs.DBCTL.bit.IN_MODE = DBA_ALL;
EPwm4Regs.DBRED.bit.DBRED = 0;
EPwm4Regs.DBFED.bit.DBFED = 0;
EPwm4_DB_Direction = DB_UP;
EPwm4Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;
EPwm4Regs.ETSEL.bit.INTEN = 1;
EPwm4Regs.ETPS.bit.INTPRD = ET_3RD;
EDIS;
}
__interrupt void epwm4_isr(void)
{
EPwm4Regs.ETCLR.bit.INT = 1;
}
// configureDAC - Configure specified DAC output
//Abänderung -->Konfiguration von zwei DACs
void configureDAC(Uint16 dac_num)
{
EALLOW;
DacaRegs.DACCTL.bit.DACREFSEL = REFERENCE;
DacaRegs.DACOUTEN.bit.DACOUTEN = 1;
DacaRegs.DACVALS.all = 0;
//DELAY_US(10); // Delay for buffered DAC to power up
DacbRegs.DACCTL.bit.DACREFSEL = REFERENCE;
DacbRegs.DACOUTEN.bit.DACOUTEN = 1;
DacbRegs.DACVALS.all = 0;
//DAC_C
DaccRegs.DACCTL.bit.DACREFSEL = REFERENCE;
DaccRegs.DACOUTEN.bit.DACOUTEN = 1;
DaccRegs.DACVALS.all = 0;
DELAY_US(10); // Delay for buffered DAC to power up
EDIS;
}
Thanks in Advanced