Part Number: TMS320F28377D
Other Parts Discussed in Thread: DESIGNDRIVE
Hello,
We have been using TI F2812 or TI F28335 in all our motor drive designs. Now the SiC power switch is the trend in the motor drive industry. SiC allows us to switch at much higher frequency (at least two times) . But this imposes more stringent requirement on the horse power (speed) of the micro-controller.
We would like to know what more powerful processors TI offers with -55 to 125C temperature rating. Otherwise we will be forced to switch to ARM or FPGA solutions.
I've looked at the TMS320F28377D-EP released. It is dual core 200Mhz but we haven't worked much with dual cores almost all of our projects are currently running on a single core DSP.
The 200Mhz will improve over our current the 150Mhz processor. The ideal candidate would be > 200 Hz single core and backward compatible with 28335 or 2812.
Are the software written for 28335 compatible with the 28377? Do we need to re-write the software to take advantage of dual processor?
What is the purpose of dual processor? To control two motors? The question is how we benefit from dual core when we just need to control one motor?
Aside from that, I noticed that the 176 pin 28377 is not compatible to 176 pin 28355.
Regards,
David