This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: InstaSPIN-Labs: Motor doesn't run as it should

Other Parts Discussed in Thread: MOTORWARE, LAUNCHXL-F28069M, BOOSTXL-DRV8305EVM

Tool/software: Code Composer Studio

hey guys,

i'm currently working with the motorware instaspin labs and the motor identification with lab2b works as it should i think. but when i'm turning the runidentify-flag back on after the identification, the motor runs not smoothly and only at very low speed. no matter which speed i enter, it runs slow and choppy. anyway the motor follows the direction which i enter, means if i put a negative speed it runs backwards and if i enter zero it stops, but it takes about 5 seconds until it follows.

in the following labs i got the same issue.

does anyone have an idea how to fix it?

thanks in advance!