Part Number: TMDSHVRESLLCKIT
Hello,
My customer purchanced a TMDSHVRESLLCKIT. But the new TMDSCNCD28027 in the kit doesn't program.
They are asking RMR. Could you please advise?
[Customer's test result]
*
A sample code for the TMDSHVRESLLCKIT was used for all the trials in this post.
*
When the CCS [bug] button was pressed, [Erasing Flash Sectors] dialog came but no progress.
Finally the dialog switched to [Erasing Flash Failed] with the console out below:
C28xx: Error occurred during flash operation: Timed out waiting for target to halt while executing FlashAPIInterface2802xV2_00.out C28xx: Error occurred during flash operation: Timed out waiting for target to halt while executing FlashAPIInterface2802xV2_00.out C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled. C28xx: File Loader: Memory write failed: Unknown error C28xx: GEL: File: C:\Users\adminuser\workspace\*****\HVLLC\F2802x_FLASH\HVLLC.out: Load failed. |
*
They have tested the newly purchased kit in some combinations.
The result tells the TMDSCNCD28027 portion has something.
*
It would be not so important, but the password was NoSecure:
- Launch TGT cfg: pass.
- Connect to the C28 core: pass.
- MemoeyBrowser 0x003F7FF8: password all-1's.
- (Load program: NG: Abort @ Erase again.)
Case study from E2E:
This thread points out a possibility of flash memory depletion.
e2e.ti.com/.../373440
Could you please advise my actions?
The first that I should do would be a depletion recovery operation.
And could you please tell me any other trials before I agree the RMR?