Part Number: TMS320F28035
Other Parts Discussed in Thread: TPS2836,
Tool/software: Code Composer Studio
Hello, TI engineer !
I am currently using TMS320F28035 as the control chip, using one PWM signal TPS2836 to generate two PWM signals with dead zone to control the BUCK circuit with synchronous rectification.I used DSP's 8 channel HRPWM signal to output the driving signal of the 8 way BUCK circuit.The switching frequency is 200K.The width of each line is 15mil.The distance between lines is 10mil.Is this spacing feasible? Will crosstalk between wired and wire occur?
As shown above, there are 8 blue lines from top to bottom.Thank you very much!