This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35H52C: EXternal watchdog reset during debugging

Part Number: F28M35H52C

Hello,

We have a custom board with a F28M35H52C micro controller  and an external watchdog that will reset the MCU if its input is not toggled within 1s. The watchdog is configured to be enabled only after we start toggling its input.

Once the watchdog is enabled, it seems not possible to debug or program the MCU with the XDS200 probe as the watchdog keeps resetting the MCU.

Is it normal behavior and is it possible to "ignore" the reset pin when the debug probe is connected ?

Thanks for the help.

Ril