Dear Ti,
My project is to generate 220V 50Hz inverter output From varing 350V-600V Input Supply.
For this i am Using "SVGEN_MF" for This Purpose. I have implemented a Equation in the Program to Maintain 220V 50Hz Inverter Out for DC Supply varing fro 350V to 600V.
I have connected an induction motor (testing purpose) at output, The Output Voltage is Maintained to 220V 50Hz , but when i increase my Supply Voltage from 350 to 600V, My Motor RPM changes 1500 to 1400. Which i am unable to understand even if my Output Voltage and Freq is Maintained.
Please Guide.
Regards,
Venky.