This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TIDM-1003: TIDM-1003: GUI for INSTASPIN and FOC

Part Number: TIDM-1003
Other Parts Discussed in Thread: MOTORWARE

Tool/software: Code Composer Studio

Hi there,

I already designed and implemented a board using the reference design "TIDM-1003". My design is a driver for 300V BLDC motor, so I changed some devices like switches, etc.

Now it's ready.

The INSTASPIN-FOC reference document is somehow strange and complicated if I want to easily run my motor.

So, is there any GUI for TIDM-1003, as I already noticed the GUI is designed for DRV boards. Do they work with custom boards or not?

And if not, is there any easy and short guide to show me how to easily identify, run and control my motor?

  • No dedicated GUI for TIDM-1003, and the GUI doesn't work for customer's board if their project changed any variables definition based example lab project. Maybe, you should use CCS to tune /debug the project easily. You might follow the TIDM guide to implement it. Or you can refer to the instaSPIN lab user's guide that can be found in the folder of motorWare.
  • I checked MotorWare for pre-designed GUIs and I found this :

    GUI Composer Runtime Installation and Webapp for MotorWare Universal GUI

    It was really useful and works with designs based on TIDM-1003.