Other Parts Discussed in Thread: TMDSCNCD28069MISO
Tool/software: Code Composer Studio
Encounterd an error at step 3.
Step 3. Connect motor, power on EVM kit,
Enable the real-time debugger again.
Set the variable “gMotorVars.Flag_enableSys” and “gMotorVars.Flag_Run_Identify” equal to 1 again.
Set the variable “gMotorVars.SpeedRef_krpm” to a different value to ensure the motor still runs.
The moment I change "gMotorVars.Flag_Run_Identify" to 1 with HV power on. Driver loses connection with the board. The picture above shows and the motor starts to rotate. At TMDSCNCD28069MISO two blue LEDs continue to be ON permanently.
Then I tried to use DC low voltage source (0V - 60V). I started with 20V, changed "gMotorVars.Flag_Run_Identify" to 1... everything fine. Slowly rised voltage to ~30-35V, same error showed up. (motor not rotating)
I am using CC version: 9.0.0.00018 clean install.
Any suggestions?