I've flashed both CPUs on the microcontroller to boot in standalone operation. When power is cycled to the microcontroller, the desired results is to have both CPUs start up and begin running. Sometimes after a power cycle, however, the microcontroller doesn't seem to begin execution. Other times, it does begin execution. I use IPCs to make sure that CPU1 has initialized and started the internal ADCs so that CPU2 can read from the registers.
Here's what's on CPU1 in main:
InitSysCtrl(); InitFlash(); // Give Memory Access to GS0/ GS14 SARAM to CPU02 // while( !(MemCfgRegs.GSxMSEL.bit.MSEL_GS0 & MemCfgRegs.GSxMSEL.bit.MSEL_GS14)) { EALLOW; MemCfgRegs.GSxMSEL.bit.MSEL_GS0 = 1; MemCfgRegs.GSxMSEL.bit.MSEL_GS14 = 1; EDIS; } IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH); Device_init(); InitCpuTimers(); // Step 2. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. InitPieVectTable(); //Enable desired GPIO Inputs and outputs here. Reference GPIO.c for guides (file excluded from build) Device_initGPIO(); // Let CPU2 know that the internal ADCs are initialized and running HWREG(IPC_BASE + IPC_O_SET) = 1UL << IPC_ADC_READY; // Wait for CPU2 to ack while((HWREG(IPC_BASE + IPC_O_STS) & (1UL << IPC_GPIO_READY))) { }
Here's what's in CPU2 main:
// Copy time critical code and Flash setup code to RAM // This includes InitFlash(), Flash API functions and any functions that are // assigned to ramfuncs section. // The RamfuncsLoadStart, RamfuncsLoadEnd, and RamfuncsRunStart // symbols are created by the linker. Refer to the device .cmd file. // #ifdef _FLASH memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize); #endif InitSysCtrl(); InitFlash(); IpcRegs.IPCBOOTSTS = C2_BOOTROM_BOOTSTS_SYSTEM_READY; // // Initialize device clock and peripherals // // Device_init(); // // Initialize GPIO and configure the GPIO pin as a push-pull output // Device_initGPIO(); // // Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts // DINT; // // Initialize PIE and clear PIE registers. Disables CPU interrupts // Interrupt_initModule(); // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // Interrupt_initVectorTable(); // // Enable Global Interrupt (INTM) and realtime interrupt (DBGM) // EINT; ERTM; InitCpuTimers(); // Wait until shared RAM is available. while((HWREGH(MEMCFG_BASE + MEMCFG_O_GSXMSEL) & (MEMCFG_GSXMSEL_MSEL_GS14 | MEMCFG_GSXMSEL_MSEL_GS15)) == 0U) { } // // Wait until CPU1 has init'd the ADC // while(!(HWREG(IPC_BASE + IPC_O_STS) & (1UL << IPC_ADC_READY))) { } // // ACK IPC flag 17 for CPU2 // HWREG(IPC_BASE + IPC_O_ACK) = 1UL << IPC_ADC_READY; HWREG(IPC_BASE + IPC_O_CLR) = 1UL << IPC_GPIO_READY;
How can I ensure that after a power cycle, both CPUs begin executing?
Thanks!