Tool/software: Code Composer Studio
Hi,
I am implementing a custom bootloader to flash firmware into my F28031 over SCI, i am listing the procedure and issue am facing. Any clue or help will be great... thanks,
- I have the complete code written to read SRECs from Motorola-2 Hex file (in Flash A)
- Am checking line CRCs and the Flash checksum.
- All the checks are good, and am jumping to the code start address in S8 record of the Hex file.
- The code seems to have jumped correctly and am getting the Application code to run.
- But for some reason, the ADC in the Application code, dosent seem to work. ADCs SOC is from EPWM1, I read ADC Result in ADCINT
- There are other ISRs in the code and they seem to work (tried gpio toggles)
- If i flash the same code in Flash B-H, the code is working fine.
Let me know where i could be going wrong..
Thanks and Regards
Santhosh Nandakumar