Part Number: LAUNCHXL-F28379D
Tool/software: Code Composer Studio
Hello all,
In below software there was a command " asm(" ESTOP0"); " . But I don't know why write it. When remove " asm(" ESTOP0"); " the AdcaResultRegs.ADCRESULT0 ( and AdcaResultRegs.ADCRESULT1; and AdcbResultRegs.ADCRESULT0; and AdcbResultRegs.ADCRESULT1;) not change.(don't sampling)
Now I have a question.
1 - Why write " asm(" ESTOP0"); " ? ( in line number 185 )
2 - When remove " asm(" ESTOP0"); " . Why sampling not happen ? ( and what I do to sampling without writing " asm(" ESTOP0"); " ?)
Thank you for helping.
//########################################################################### // // FILE: adc_soc_software_cpu01.c // // TITLE: ADC software triggering for F2837xD. // //! \addtogroup cpu01_example_list //! <h1> ADC SOC Software Force (adc_soc_software)</h1> //! //! This example converts some voltages on ADCA and ADCB based on a software //! trigger. //! //! After the program runs, the memory will contain: //! //! - \b AdcaResult0 \b: a digital representation of the voltage on pin A2\n //! - \b AdcaResult1 \b: a digital representation of the voltage on pin A3\n //! - \b AdcbResult0 \b: a digital representation of the voltage on pin B2\n //! - \b AdcbResult1 \b: a digital representation of the voltage on pin B3\n //! //! Note: The software triggers for the two ADCs happen sequentially, so the //! two ADCs will run asynchronously. //! // //########################################################################### // $TI Release: F2837xD Support Library v3.06.00.00 $ // $Release Date: Mon May 27 06:48:24 CDT 2019 $ // $Copyright: // Copyright (C) 2013-2019 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //########################################################################### // // Included Files // #include "F28x_Project.h" // // Function Prototypes // void ConfigureADC(void); void SetupADCSoftware(void); // // Globals // Uint16 AdcaResult0; Uint16 AdcaResult1; Uint16 AdcbResult0; Uint16 AdcbResult1; void main(void) { // // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the F2837xD_SysCtrl.c file. // InitSysCtrl(); // // Step 2. Initialize GPIO: // This example function is found in the F2837xD_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts // DINT; // // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the F2837xD_PieCtrl.c file. // InitPieCtrl(); // // Disable CPU interrupts and clear all CPU interrupt flags: // IER = 0x0000; IFR = 0x0000; // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in F2837xD_DefaultIsr.c. // This function is found in F2837xD_PieVect.c. // InitPieVectTable(); // // Enable global Interrupts and higher priority real-time debug events: // EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM // //Configure the ADCs and power them up // ConfigureADC(); // //Setup the ADCs for software conversions // SetupADCSoftware(); // //take conversions indefinitely in loop // do { // //convert, wait for completion, and store results //start conversions immediately via software, ADCA // AdcaRegs.ADCSOCFRC1.all = 0x0003; //SOC0 and SOC1 // //start conversions immediately via software, ADCB // AdcbRegs.ADCSOCFRC1.all = 0x0003; //SOC0 and SOC1 // //wait for ADCA to complete, then acknowledge flag // while(AdcaRegs.ADCINTFLG.bit.ADCINT1 == 0); AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; // //wait for ADCB to complete, then acknowledge flag // while(AdcbRegs.ADCINTFLG.bit.ADCINT1 == 0); AdcbRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; // //store results // AdcaResult0 = AdcaResultRegs.ADCRESULT0; AdcaResult1 = AdcaResultRegs.ADCRESULT1; AdcbResult0 = AdcbResultRegs.ADCRESULT0; AdcbResult1 = AdcbResultRegs.ADCRESULT1; // //at this point, conversion results are stored in //AdcaResult0, AdcaResult1, AdcbResult0, and AdcbResult1 // // //software breakpoint, hit run again to get updated conversions // asm(" ESTOP0"); }while(1); } // // ConfigureADC - Write ADC configurations and power up the ADC for both // ADC A and ADC B // void ConfigureADC(void) { EALLOW; // //write configurations // AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4 AdcbRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4 AdcSetMode(ADC_ADCA, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE); AdcSetMode(ADC_ADCB, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE); // //Set pulse positions to late // AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1; AdcbRegs.ADCCTL1.bit.INTPULSEPOS = 1; // //power up the ADCs // AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1; AdcbRegs.ADCCTL1.bit.ADCPWDNZ = 1; // //delay for 1ms to allow ADC time to power up // DELAY_US(1000); EDIS; } // // SetupADCSoftware - Setup ADC channels and acquisition window // void SetupADCSoftware(void) { Uint16 acqps; // // Determine minimum acquisition window (in SYSCLKS) based on resolution // if(ADC_RESOLUTION_12BIT == AdcaRegs.ADCCTL2.bit.RESOLUTION) { acqps = 14; //75ns } else //resolution is 16-bit { acqps = 63; //320ns } // //Select the channels to convert and end of conversion flag //ADCA // EALLOW; AdcaRegs.ADCSOC0CTL.bit.CHSEL = 2; //SOC0 will convert pin A2 AdcaRegs.ADCSOC0CTL.bit.ACQPS = acqps; //sample window is acqps + //1 SYSCLK cycles AdcaRegs.ADCSOC1CTL.bit.CHSEL = 3; //SOC1 will convert pin A3 AdcaRegs.ADCSOC1CTL.bit.ACQPS = acqps; //sample window is acqps + //1 SYSCLK cycles AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 1; //end of SOC1 will set INT1 flag AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared //ADCB AdcbRegs.ADCSOC0CTL.bit.CHSEL = 2; //SOC0 will convert pin B2 AdcbRegs.ADCSOC0CTL.bit.ACQPS = acqps; //sample window is acqps + //1 SYSCLK cycles AdcbRegs.ADCSOC1CTL.bit.CHSEL = 3; //SOC1 will convert pin B3 AdcbRegs.ADCSOC1CTL.bit.ACQPS = acqps; //sample window is acqps + //1 SYSCLK cycles AdcbRegs.ADCINTSEL1N2.bit.INT1SEL = 1; //end of SOC1 will set INT1 flag AdcbRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag AdcbRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared EDIS; } // // End of file //