Tool/software: Code Composer Studio
Hi,
I am using eZdsp TMS320F28335 board for testing ADC channel.
Test conditions are :
- input = 2.4 V p-p sine wave @ 50 KHz
- Sampling rate 1 mbps
When I tried sampling channel at 1 mbps using PWM as source of trigger for SOC, the sine wave read in debug mode not coming as sine instead it is coming as triangular wave.
Is there any other way with which we can configure the sampling frequency other that PWM time base register. What is the maximum sampling frequency that we can configure?
I am not getting exactly why the ADC is not reading sine wave properly at the rate of 1mbps.
Please help with the issue.
Thanks,
Namita